BCM43340 Broadcomm WLAN support on IMX6Q Platform which is running with Android Pie (9.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCM43340 Broadcomm WLAN support on IMX6Q Platform which is running with Android Pie (9.0)

Jump to solution
695 Views
ramakrishna_n
Contributor I

Hello NXP Team,

   We are working on a custom platform which is having IMX6Q as the SOC. The platform have BCM43340 Broadcom WLAN/BT module. As we are porting to the Android Pie sources which we are downloaded from NXP SABRESD platform, we are observing that the Linux kernel (Version 4.14 ) does not have support for BCM43340(there is no folder name "bcmdhd" in the path drivers/net/wireless).

   However there is support for bcmdhd in Yocto project Kernel (version 4.9) for IMX6Q but if we are porting these module to android Linux kernel we are facing severe compilation issues(seems some network core structures got changed from 4.9 to 4.14)

   Is there any repositories or support available for bcmdhd in Android Pie kernel release for IMX6Q? Requesting your help on this.

Regards,

Ramakrishna Nimmala

Labels (2)
0 Kudos
1 Solution
660 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies but on version 4.14 it is not supported due to Marvel's introduction.

Thank you for your comprehension.

BR,

Ivan.

View solution in original post

0 Kudos
1 Reply
661 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies but on version 4.14 it is not supported due to Marvel's introduction.

Thank you for your comprehension.

BR,

Ivan.

0 Kudos