BC3770 works for SCM-i.MX 6Quad chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BC3770 works for SCM-i.MX 6Quad chip

794 Views
sunjianxin66
Contributor II

Dear NXP support!

I am wondering if a BC3770 will provide enough current for SCM-i.MX6Quad Single Chip Module. From the reference design of the module(SPF-28927.pdf page 2) it says the total SCM current requirements is 2045 mA. But on the datasheet of BC3770(MC32BC3770.pdf page 1) says "Up to 2.0 A load current for system or battery". They are close.

I really want to use these 2 parts together. Could you please confirm me that if I can use them together?

Thank you very much!

Labels (4)
0 Kudos
1 Reply

514 Views
igorpadykov
NXP Employee
NXP Employee

Hi JIANXIN

datasheet provides max. currents based on special tests which usually are

not used in typical customer applications. So one can consider that pmic as suitable

for this scm module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos