BAR4 and BAR5 can not be accessed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BAR4 and BAR5 can not be accessed

1,108 Views
masamiyasui
Contributor I

BAR4 and BAR5 of Endpoint on i.MX6Q can not be accessed from Root Complex.
BAR 0 to BAR 3 are accessible without problems.
Is there any restriction on BAR 4 and BAR 5 of i.MX6Q?


I compared the behavior when only two BARs are enabled.

In the following three cases, the memory space allocated on the Root Complex side is the same.

[case 1]

   BAR 0: 32 bit memory 1 MB -> OK
   BAR 2: 32 bit memory 1 MB -> OK


[case 2]
   BAR 0: 32 bit memory 1 MB -> OK
   BAR 4: 32 bit memory 1 MB -> NG


[case 3]
   BAR 0: 32 bit memory 1 MB -> OK
   BAR 5: 32 bit memory 1 MB -> NG

Labels (2)
0 Kudos
Reply
2 Replies

909 Views
igorpadykov
NXP Employee
NXP Employee

Hi Masami

please refer to bar differencies described on

https://community.nxp.com/thread/387557?commentID=630870#comment-630870 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

909 Views
masamiyasui
Contributor I

Hello, igorpadykov, thank you for your cooperation.


In the presented information, there was an example using BAR 4 or BAR 5 as the I / O area.


Is there any example that BAR 4 or BAR 5 can be used as a memory area?

Best regards
Masami

0 Kudos
Reply