Avilavility of i.MX6S PCIeGEN2 port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Avilavility of i.MX6S PCIeGEN2 port

1,140 Views
torus1000
Contributor V

Hi,

We have plan to use mSATA or CFast devices.

Is it possible to connect them to the i.MX6S PCIeGEN2 port?

I only concern about physical layer and I do not mention about drivers at this point.

Is there any difficulty for it?

Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,071 Views
art
NXP Employee
NXP Employee

The PCIe port of the i.MX6Solo processor is compliant with the PCIe Gen.2 specification at the speeds of up to 5Gbit/s. So, there should be no any problem.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,071 Views
torus1000
Contributor V

Dear Autur,

Just in case, I want to confirm one more time.

I checked pin assignment of mPCIe nad mSATA. Please see attached materials.

As far as I know, some PCs actually has dual roll slot(mPCIe and mSATA).

Does i.MX6DL-SabreSD also support both?

In another word, does i.MX6 PCIe support SATA I/F too?


Thanks.

---

mPCIe_mSATA52_2.pngmPCIe_mSATA52.png

0 Kudos
Reply

1,071 Views
art
NXP Employee
NXP Employee

No, the Mini-PCIe connector of the i.MX6DL SABRE SD board does not support Mini-SATA. There is a separate SATA connector on the board.

Best Regards,

Artur

0 Kudos
Reply