Availability of i.MX6 Linux VPU API

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Availability of i.MX6 Linux VPU API

Jump to solution
7,174 Views
MickeyI
Contributor III

Hi,

Is there a i.MX6 Linux VPU API available for download? All I could find is one for i.MX51.

Thanks,

Mickey.

Labels (1)
Tags (1)
1 Solution
3,117 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE

View solution in original post

0 Kudos
Reply
6 Replies
3,118 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE

0 Kudos
Reply
3,117 Views
brainmeltdown
Contributor I

Seems like the document you linked to (and others like it for different cores) do not mention the C header file(s) that my application must #include.  What is it?  And do you have any example/demo code to build with Yocto that uses the VPU API?

0 Kudos
Reply
3,117 Views
jimmychan
NXP TechSupport
NXP TechSupport

In the latest BSP documentation, there is a PDF file i.MX_VPU_Application_Programming_Interface_Linux_Reference_Manual.pdf. You can take this for reference.

0 Kudos
Reply
3,117 Views
maxj
Contributor I

Is there a different link to use for this document?  Or can anyone attach the bundle to the discussion?  When I try to access the page, I get this:

Error 500--Internal Server Error

From RFC 2068 Hypertext Transfer Protocol -- HTTP/1.1:

10.5.1 500 Internal Server Error

The server encountered an unexpected condition which prevented it from fulfilling the request.

0 Kudos
Reply
3,115 Views
Yuri
NXP Employee
NXP Employee

Please try the enclosed.

0 Kudos
Reply
3,115 Views
maxj
Contributor I

Got it!  Thanks.

0 Kudos
Reply