We are working on an IMX8MMINI board with ADV7535 MIPI-DSI to HDMI chip, and we have met a problem.
SoC: IMX8MMINI
Display chip: ADV7535
Display interface: HDMI
O/S: Android 9 or 10
Kernel version: 4.14.98 or 5.4.70
Main issue:
We have different types of displays, and we want to use them with the same board, and we do not want to change the display setting in the software.
We set the default resolution in Android at 1080p, but it could not be displayed on a 720p display only when we set the default resolution to 720p.
What we would like to do is the device could be displayed on both 1080p and 720 resolution displays separately.
As we know, ADV7535 could support EDID detection, it could detect the EDID provided from the display and provide the correct resolution, so we would like to use this function; however, when we use the resources provided from NXP(BSP/Device tree), it could not be achieved.
We have checked with Analog Device about this issue, and they provided us with a script file, but we still need an example code for reference.
Could anyone help with this?
Thanks.