Audio recording "overun" issue in AC97 codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio recording "overun" issue in AC97 codec

Jump to solution
538 Views
yashavanthashet
Contributor V

Hi all,

We are using imx_"3.14.38_6qp_ga yocto fido" bsp in our custom board.

Here sometimes we are facing issue in audio recording. while recording its showing below print.

"overrun!!! (at least 1.921 ms long)".

command used to record is "arecord -d 10 test.wav". This issue is present only in AC97 audio codec.

Could anybody help me to solve this.

Thanks in advance.

Regards,

Yashavantha

Labels (4)
0 Kudos
1 Solution
432 Views
Yuri
NXP Employee
NXP Employee

Hello,

   I an afraid the issue  concerns with Linux file system performance.

You may try using SD card of class 10 or /dev/shm node for RAMFS for relatively

short files.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
433 Views
Yuri
NXP Employee
NXP Employee

Hello,

   I an afraid the issue  concerns with Linux file system performance.

You may try using SD card of class 10 or /dev/shm node for RAMFS for relatively

short files.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos