Hello ,
I am working on a custom board based on imx6q-arm2 board. I have linux-imx 3.14.28 running on it. I am facing an issue in AUDIO. My board has TLV codec interfaced via audmux to ssi. When i use aplay command , it shows the error as
aplay: pcm_write:1947: write error: Input/output error
and dmesg shows
[ 6834.037168] imx-sdma 20ec000.sdma: wml = 0x0000001a
[ 6834.037181] imx-sdma 20ec000.sdma: shp_addr = 0x02028000
[ 6834.037193] imx-sdma 20ec000.sdma: per_addr = 0x00000000
[ 6834.037205] imx-sdma 20ec000.sdma: event_mask0 = 0x00000000
[ 6834.037217] imx-sdma 20ec000.sdma: event_mask1 = 0x00000040
[ 6834.037244] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 0: count: 16384 dma: 0x4c7c0000 intr
[ 6834.037261] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 1: count: 16384 dma: 0x4c7c4000 intr
[ 6834.037277] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 2: count: 16384 dma: 0x4c7c8000 intr
[ 6834.037293] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 3: count: 16384 dma: 0x4c7cc000 wrap intr
[ 6844.037593] ALSA sound/core/pcm_lib.c:1947 playback write error (DMA or IRQ trouble?)
So what exactly can be the cause of this error.
If i use aplay -M test.wav , this playback error does not show up. but still sound can not be heard. Also with -M option, aplay never exists.
-Thanks
Sharvari Harisangam.
Hi Sharvari
seems dts files for arm2 board, like imx6q-arm2.dts, do not have
ssi entries. Suggest to add them using SabreSD dts examples
linux-2.6-imx.git - Freescale i.MX Linux Tree
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I have added ssi block in DTS tree. I have also verified from dmesg logs that ssi block is getting initialized correctly. From the above logs shared, last line suggests error in DMA or IRQ. How can I check this?