Audio Capabilities of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio Capabilities of i.MX6UL

1,024 Views
agodeau
Contributor III

Hi,

 I was wondering if the i.MX6UL has any audio capabilities, it is not clear from the documentation I have. I am looking to implement a speaker and need to know if I need an additional IC.

Thanks

Labels (2)
Tags (2)
2 Replies

876 Views
linda_zhang
Contributor IV

We are using MYIR's MYD-Y6ULX development board. The audio is brought out through I2S.

audio.png

876 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Aquiel Godeau,

You can see on the i.MX6UL datasheet (link below) that this processor has a SAI module which provides a synchronous audio interface (SAI) that supports full duplex serial interfaces with frame synchronization, such as I2S, AC97, TDM, and codec/DSP interfaces.

https://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

This means that while it does have audio capabilities you would need to add a codec to which you can connect an audio jack or a speaker (with amplification if desired).

You can see the i.MX6UL EVK for an example of how audio is implemented.

I hope this helps!

Regards,

0 Kudos