Athereos wifi driver fails during boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Athereos wifi driver fails during boot

1,669件の閲覧回数
ArifKhan
Contributor I
Hi, I am working on SABRE TABLET board with "L2.6.35_11.05.01_ER_source" BSP, I am able to bring up the board and boot from the SD card, I compiled the wifi driver as Module and loaded the module as below root@freescale ~$ cd /lib/modules/2.6.35.3-998-ga1cd8a7 root@freescale /lib/modules/2.6.35.3-998-ga1cd8a7/kernel/drivers/staging$ ls ath6kl root@freescale /lib/modules/2.6.35.3-998-ga1cd8a7/kernel/drivers/staging$ cd </2.6.35.3-998-ga1cd8a7/kernel/drivers/staging$ cd ath6kl/ <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ ls ath6kl.ko <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ modprobe ath6kl.ko ath6kl: module is from the staging directory, the quality is unknown, you have been warned. <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ AR6000: Unsupported configuration opcode: 3 AR6000: Unsupported configuration opcode: 3 HIF Interrupt processing is SYNC ONLY AR6000: Unsupported configuration opcode: 7 AR6000: Unsupported configuration opcode: 5 In aggr_init.. going out of aggr_init..status OK Unknown firmware revision: 805307778 ar6000_avail: ar6000_sysfs_bmi_get_config failed <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ <6.35.3-998-ga1cd8a7/kernel/drivers/staging/ath6kl$ Its fails giving error "ar6000_avail: ar6000_sysfs_bmi_get_config failed" I am not sure How to solve it, has any one tried enabling wifi driver. Arif
0 件の賞賛
返信
2 返答(返信)

1,325件の閲覧回数
ArifKhan
Contributor I
0 件の賞賛
返信

1,325件の閲覧回数
Swamy
Contributor III

Hi Arif,

I am also facing the same issue, if you have found the solution, can you share it please.

Regards,

Swamy

0 件の賞賛
返信