[Arrow/i.MX8MN/Linux L5.4.3_1.0.0]TensorFlow lite Acceleration issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Arrow/i.MX8MN/Linux L5.4.3_1.0.0]TensorFlow lite Acceleration issues

ソリューションへジャンプ
1,344件の閲覧回数
Lambert
NXP Employee
NXP Employee

 

Project info are below shown:

Software: BSP 5.4.3_1.0.0  (tensorflow + keras)

Hardware: imx8m nano, pico zense Dcam710(USB)

Pls refer to attached for detail.

ラベル(1)
0 件の賞賛
1 解決策
1,329件の閲覧回数
DevinJiao
NXP Employee
NXP Employee

Hi Lambert,

We don't have optimization for OpenCL in OpenCV. If customer wants to get a better performance, running OpenCV on CPU is a good option.

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,330件の閲覧回数
DevinJiao
NXP Employee
NXP Employee

Hi Lambert,

We don't have optimization for OpenCL in OpenCV. If customer wants to get a better performance, running OpenCV on CPU is a good option.

0 件の賞賛