Argon imx6ul SOM hang issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Argon imx6ul SOM hang issue

594 Views
hardikbehere
Contributor I

We are facing following issue “argon imx6ul” SOM .

SOM gets hang if Ethernet is disable in device tree and menu config.

But if we connect pen-drive in same image (with disabled Ethernet in device tree) , then we are not facing SOM hang issue.

we are using kernel version 4.1.15-1.2.0+g77f6154.

Labels (1)
Tags (1)
0 Kudos
1 Reply

524 Views
igorpadykov
NXP Employee
NXP Employee

Hi hardik

to check if this is specifc for that board, please try to reproduce issue

on nxp i.MX6UL EVK reference board with official nxp releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

one can check using core-image-minimal image described in

Table 1. Freescale Yocto project images attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos