Are there lot to lot difference with iMX6 solo??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there lot to lot difference with iMX6 solo??

Jump to solution
981 Views
takafuminaka
Contributor II

There is a problem with our product.

When we made prototype with iMX6 Solo (lot No. 1313), there was no problem.
They work properly.

When we began mass production with same board and iMX6 Solo (lot no.1351),
this problem occurred.
The data we stored in DDR3 SDRAM definitely changes.
The probability of this problem is clearly difference between lots as below.

Lot No.  probability
1313   0%
1351  33%
1403  90%

This level of defectiveness is nothing short of extraordinary.

There is no change with software.
The difference is lot No. only.

Do we need to change some settings regarding DDR memory depends on CPU lot?
For example, are there any lot to lot differences about MPU configuration?
Is the latest Reference manual Rev. 1, 04/2013 ?
We immediately need even small bits of information.

This problem has huge impact on our production now.
Do you know something about this?

best regards,

Naka

Labels (2)
Tags (2)
1 Solution
664 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

please run DDR tests below and find new calibrations settings

https://community.freescale.com/message/331721#331721

https://community.freescale.com/docs/DOC-96412

Also issue may be related to improper soldering process.

One can try to resolder chips.

Other items for checking is given in

IMX6DQ6SDLHDG

IMX6DQ6SDLHDG, Hardware Development Guide

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

please run DDR tests below and find new calibrations settings

https://community.freescale.com/message/331721#331721

https://community.freescale.com/docs/DOC-96412

Also issue may be related to improper soldering process.

One can try to resolder chips.

Other items for checking is given in

IMX6DQ6SDLHDG

IMX6DQ6SDLHDG, Hardware Development Guide

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

664 Views
takafuminaka
Contributor II

0 Kudos
664 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

yes it is possible to use WFI instruction with iMX6 Solo processor,

however seems you should create new thread for this problem.

Please provide details what BSP was used. How test was performed.

Best regards

chip

0 Kudos