Hi all,
Are there any recommended oscillator or operability confirmed oscillator for i.MX6 ?
My customer will use oscillator for 24MHz clock of i.MX6SL.
I read following threads but I could only get information on frequency deviation without the recommended circuit diagram.
https://community.nxp.com/message/594692
https://community.nxp.com/message/411963
https://community.nxp.com/message/431129
https://community.nxp.com/message/458924
Furthermore, this EB is mentioned only for crystal.
https://www.nxp.com/docs/en/engineering-bulletin/EB830.pdf
Please someone share the information about recommended oscillator or operability confirmed oscillator for i.MX6.
Ko-hey
Solved! Go to Solution.
Hi Ko-hey
>Could you give us an opinion for it ?
I think Your considerations are correct. Sorry I have no other suggestion.
I think customer can add to this device level converter or try to find other device
with appropriate characteristics.
Best regards
igor
Hi Ko-hey
>Could you give us an opinion for it ?
I think Your considerations are correct. Sorry I have no other suggestion.
I think customer can add to this device level converter or try to find other device
with appropriate characteristics.
Best regards
igor
Hi Ko-hey
one can try oscillator used in i.MX6UL EVK :
Buy NZ2520SH-24MHZ ERG3199A, Nihon Dempa Kogyo Co., Ltd. (NDK), ED Inventory
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thank you for reply.
Where is it in i.MX6UL EVK ? I can't find it in following schematic.
https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES
Ko-hey
Hi Ko-hey
Y503 please check BOM in
Best regards
igor
hi, igorpadykov
Thank you for reply.
I understand EVK has 24MHz oscillator but I think it's not match for DC parameters of XTALI in i.MX6.
According to the datasheet of i.MX6, the XTALI high-level DC input voltage is from 0.8 x NVCC_PLL to NVCC_PLL V.
Furthermore, the nominal default setting as 1.1 V.
As a result, the XTALI high-level DC input voltage is from 0.88 to 1.1 V.
On the other hand, the specification of the device is as below..
Supply Voltage [VCC] (V) | +1.8 to +3.3 (*1) | |
VOL Max. / VOH Min. (V) | 0.1 VCC / 0.9 VCC | 0.2 VCC / 0.8 VCC |
https://www.ndk.com/en/products/search/clock/1190899_1433.html
Even if user select minimum supply voltage (Voh Min is 1.62 V), I think that it doesn't match the specification for i.MX6 XTALI.
Could you give us an opinion for it ?
Ko-hey