Are there Linux OS for i.MX6Q SABRESDB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there Linux OS for i.MX6Q SABRESDB?

1,276件の閲覧回数
joowonkim
Contributor III

Hi all.

I want install the linux on i.MX6Q SABRESDB board.

So I looking Linux OS for i.MX6Q SABRESDB.

Are there Linux for i.MX6Q SABRESDB?

Best regards!

JooWon.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,059件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

Hi, JooWon

Firstly, open the link followed:

i.MX 6Quad SABRE Development Board|NXP

Secondly, download the gz file named "L4.1.15_1.1.0_LINUX_DOCS " in the Recommended Documentation.

Thirdly, unzip the file and follow the file "Freescale_Yocto_Project_User's_Guide.pdf" to build a Yocto image and use MFG_TOOL to download to the i.MX6Q SABRE-SDB. The MFG_TOOL is named “IMX6_L4.1.15_1.1.0_MFG_TOOL(REV L4.1.15_1.1.0)” in the Programmers (Flash, etc.) which attached in the following link:

i.MX 6Quad SABRE Development Board|NXP

(PS: The MFG_TOOL contains the built Yocto image, So you can directly step to Thirdly to run MFG_TOOL to download the Yocto image to your i.MX6Q SABRE-SDB.)

All the best

Jian Jiang

0 件の賞賛
返信

1,059件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

You can get the documentation from this link:

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&appType=license&location...

User guide (how to install), release notes and multimedia docs for your linux installation

0 件の賞賛
返信

1,059件の閲覧回数
saurabh206
Senior Contributor III

Linux OS is supported, you can find it from following link

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Go to Run Time software.

0 件の賞賛
返信