Are the muxed I/O signals shared with CAN still available for the 'No CAN' i.MX 7 dual core options?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the muxed I/O signals shared with CAN still available for the 'No CAN' i.MX 7 dual core options?

583 Views
johnathanfeuers
Contributor II

For the processor options like MCIMX7D3EVK10SD that do NOT support CAN, the other shared muxed I/O at the processor balls are still available correct?

It seems like that is the case, but I had trouble finding confirmation in the TRM/datasheet. So I just wanted to confirm this.

Labels (1)
0 Kudos
Reply
1 Reply

491 Views
igorpadykov
NXP Employee
NXP Employee

Hi Johnathan

yes correct, in this case other shared muxed I/O at the processor balls are still available.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply