Are the following camera options feasible?

cancel
Showing results for 
Search instead for 
Did you mean: 

Are the following camera options feasible?

250 Views
andy5
Contributor I

Are the following camera options feasible? In this scheme, the sensor signal is transmitted to the Mipi CSI interface of imx8qm through one lane LVDS of data, one lane LVDS of clock and one lane LVDS of synchronization signal.But the Mipi_CSI interface of imx8qm seems to be only used to receive data.

pastedImage_2.png

The problem is as follows:

The four lane channels of MIPI_CSI seem to be used to receive data. Now I want to use one lane of the Mipi_CSI lanes as the sensor data receive lane and other one lane to be used as the Synchronous signal receive lane, is it feasible? 

Thank you for the answering the above question!

Tags (1)
0 Kudos
2 Replies

175 Views
b45499
NXP TechSupport
NXP TechSupport

pastedImage_1.png

0 Kudos