Are the following camera options feasible? In this scheme, the sensor signal is transmitted to the Mipi CSI interface of imx8qm through one lane LVDS of data, one lane LVDS of clock and one lane LVDS of synchronization signal.But the Mipi_CSI interface of imx8qm seems to be only used to receive data.
The problem is as follows:
The four lane channels of MIPI_CSI seem to be used to receive data. Now I want to use one lane of the Mipi_CSI lanes as the sensor data receive lane and other one lane to be used as the Synchronous signal receive lane, is it feasible?
Thank you for the answering the above question!