Are FBK: commands with the uuu tool supported on i.MX6 ULL ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are FBK: commands with the uuu tool supported on i.MX6 ULL ?

3,976件の閲覧回数
dallasfoley
Contributor I

I can successfully load u-boot, .dtb, zImage and initramfs with the uuu tool's SDP: commands from my linux host.

However, I'm not sure how to run FBK: comands. I just get 'Wait for Known USB' as a response.

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

3,524件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dallas

yes it is supported, one can look at documentation

UUU default support protocol list · NXPmicro/mfgtools Wiki · GitHub 

https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,524件の閲覧回数
dallasfoley
Contributor I

Thanks, I mostly have it working Ok now

0 件の賞賛
返信

3,524件の閲覧回数
dallasfoley
Contributor I

I can't seem to get the FB: commands working for u-boot.

I have the fastboot command running in u-boot and my usb device shows up on my host, but the command fails.

./uuu u-boot-dtb.imx

./uuu -s

U>FB: ucmd help
1:2>Start Cmd:FB: ucmd help
New USB Device Attached at 1:2
1:2>Fail Bulk(W):LIBUSB_ERROR_TIMEOUT(0.001s)
Bulk(W):LIBUSB_ERROR_TIMEOUT

0 件の賞賛
返信

3,524件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can look at example_kernel_emmc.uuu included in

Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dual

Best regards
igor

0 件の賞賛
返信