Since the Arduino Interface on the MIMXRT1050-EVK is not populated I would like to know what do I need to integrate mzself the hardware on the board.
I will for sure need the Arduinio stackable header but the question is if I need anz other hardware component to be solded on the board. As I have seen on the schematics there are some 0 Ohm resistors with the label DNP (Do not place) on some of the pins of the header. Do I need to sold them in case I integrate the Arduino Interface?