Arduino header on i.MX6UltraLite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Arduino header on i.MX6UltraLite

Jump to solution
1,847 Views
giulianofranche
Contributor II


Hi

we would like to test the i.MX6UltraLite, but we have a pretty simple question: do we have to solder anything in the arduino header to plug some shields in?

The picture of the board shows that the JTAG connector is in the arduino header area, and I'm afraid I may not have enough space to plug the shield directly on the board

Regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,702 Views
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

View solution in original post

0 Kudos
Reply
3 Replies
1,702 Views
giulianofranche
Contributor II

Thank you for your answer Artur.

Do we must solder the extenders, or is this optionnal?

0 Kudos
Reply
1,703 Views
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

0 Kudos
Reply
1,702 Views
art
NXP Employee
NXP Employee

Yes, you can solder some connector extenders into the Arduino header pads to leave more space under the shield.

Best Regards,

Artur

0 Kudos
Reply