Appropriate termination for unused DDR3 pins on a i.MX6 dual/quad design with 32-bit bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Appropriate termination for unused DDR3 pins on a i.MX6 dual/quad design with 32-bit bus

Jump to solution
880 Views
greglepley
Contributor I

Hello,

We are looking to create a line of products that utilize i.MX6 Solo, Dual, and Quad processors. Our desire is to change as little as possible in layout between each variant of the iMX6. The Solo provides support for a 32-bit DDR3 bus and the other 32-bits are left NC according to documentation for the Solo. For the time being, we would like to keep the 32-bit bus implemented in the Dual and Quad variants as well with the option of moving to 64-bits at a later date. What are the appropriate actions to take with the unused 32 data lines on the Dual/Quad processors? Is it safe to leave them NC and floating or should we tie them high or low? We cannot find documentation that provides the appropriate design rules for this situation.

Thank you,

Gregory

Labels (3)
0 Kudos
1 Solution
592 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gregory

unused ddr pins can be left unconnected.

Best regards

igor
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
593 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gregory

unused ddr pins can be left unconnected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos