App with curl dependency on IMX6 - Board fails to boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

App with curl dependency on IMX6 - Board fails to boot

1,582件の閲覧回数
senthilacs
Contributor I

I created a simple application which uses curl to download a file. In my Makefile.am, I added
LDFLAGS = -lcurl

and in myapp.bb, I added
DEPENDS = curl

I added my app in local.conf as
IMAGE_INSTALL_append += “myapp”

The build went fine and when I try to boot on a IMX6 board, it refuses to boot. If I remove all the curl dependencies, it boots fine.

Has anyone tried an app with curl and been able to boot properly? If you see any other steps that I am missing here, can you help me out please?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,262件の閲覧回数
b36401
NXP Employee
NXP Employee

What exact error message you are getting on boot?

Have a great day,

Victor

0 件の賞賛
返信

1,262件の閲覧回数
senthilacs
Contributor I

Hi Victor,

We got the logs through the serial port and we see this

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.                                                                 See Linux Documentation/init.txt for guidance.

Serial Port logs Full

================

U-Boot 2015.07-00111-g5981a23 (Nov 11 2015 - 16:02:50 -0700)

CPU:   Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)

Reset cause: POR

Board: SABRE Lite

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB

auto-detected panel 1280x720M@60

Display: hdmi:1280x720M@60 (1280x720)

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 6

FEC [PRIME], usb_ether

Error: usb_ether address not set.

Hit any key to stop autoboot:  0

AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode

flags: ncq stag pm led clo only pmp pio slum part

No port device detected!

** Bad device size - sata 0 **

SATA device 1: unknown device

** Bad device sata 1 **

MMC: no card present

MMC: no card present

** Bad device mmc 0 **

switch to partitions #0, OK

mmc1 is current device

reading /6x_bootscript

4092 bytes read in 13 ms (306.6 KiB/s)

## Executing script at 10008000

reading uEnv.txt

** Unable to read file uEnv.txt **

Setting bus to 1

Valid chip addresses: 50

Setting bus to 2

Valid chip addresses:

------ no Freescale display

Valid chip addresses:

------ no ft5x06 touch controller

Valid chip addresses:

------ no ILI210x touch controller

Valid chip addresses:

------ no 800x480 display

reading /imx6q-sabrelite.dtb

47367 bytes read in 19 ms (2.4 MiB/s)

only CEA modes allowed on HDMI port

reading /uImage

4407008 bytes read in 218 ms (19.3 MiB/s)

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.10.17-1.0.2_ga+yocto+g4d

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    4406944 Bytes = 4.2 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 12000000

   Booting using the fdt blob at 0x12000000

   Loading Kernel Image ... OK

   Using Device Tree in place at 12000000, end 1200e906

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 3.10.17-1.0.2_ga+yocto+g4da158a (srini@srini-VirtualBox) (gcc vers                                                                ion 4.9.1 (GCC) ) #1 SMP Wed Jan 27 04:19:45 EST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Qua                                                                d SABRE Lite Board

cma: CMA: reserved 256 MiB at 26000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @c1059000 s8704 r8192 d15872 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260928

Kernel command line: enable_wait_mode=off video=mxcfb0:dev=hdmi,1280x720M@60,if=                                                                RGB24 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=28M console=ttymx                                                                c1,115200 vmalloc=400M consoleblank=0 rootwait root=/dev/mmcblk0p2 mxc_hdmi.only                                                                _cea=1

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1024MB = 1024MB total

Memory: 768196k/768196k available, 280380k reserved, 425984K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xe6800000 - 0xff000000   ( 392 MB)

    lowmem  : 0xc0000000 - 0xe6000000   ( 608 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc0757024   (7485 kB)

      .init : 0xc0758000 - 0xc079d200   ( 277 kB)

      .data : 0xc079e000 - 0xc07db860   ( 247 kB)

       .bss : 0xc07db860 - 0xc084087c   ( 405 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32470000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0xc059aa28 - 0xc059aa80

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1125 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2425 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV at 1150 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

1P8V: 1800 mV

2P5V: 2500 mV

3P3V: 3300 mV

usb_otg_vbus: 5000 mV

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@l                                                                inux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Switching to clocksource mxc_timer1

imx6q-pcie 1ffc000.pcie: phy link never came up

imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x1000-0x10000]

pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

pci_bus 0000:00: root bus resource [bus 00-ff]

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

pureg-dummy: no parameters

imx6_busfreq busfreq.15: DDR medium rate not supported.

Bus freq driver module loaded

bounce pool size: 64 pages

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

squashfs: version 4.0 (2009/01/31) Phillip Lougher

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

fuse init (API version 7.22)

msgmni has been set to 1180

Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_sdc_fb fb.26: register mxc display driver hdmi

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1280x720@60: CVT Name - .921M9

mxc_sdc_fb fb.26: 1280x720 h_sync,r,l: 40,110,220  v_sync,l,u: 5,5,20 pixclock=7                                                                4250000 Hz

imx-ipuv3 2800000.ipu: try ipu internal clk

imx-ipuv3 2800000.ipu: disp=0, pixel_clk=74250000 74250000 parent=74250000 div=1

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

mxc_sdc_fb fb.26: 1280x720 h_sync,r,l: 40,110,220  v_sync,l,u: 5,5,20 pixclock=7                                                                4250000 Hz

imx-ipuv3 2800000.ipu: try ipu internal clk

imx-ipuv3 2800000.ipu: disp=0, pixel_clk=74250000 74250000 parent=74250000 div=1

Console: switching to colour frame buffer device 160x45

mxc_sdc_fb fb.27: mxcfb1 is turned off!

mxc_sdc_fb fb.28: mxcfb2 is turned off!

mxc_sdc_fb fb.29: mxcfb3 is turned off!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

console [ttymxc1] enabled

serial: Freescale lpuart driver

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

mxc_sdc_fb fb.26: 640x480 h_sync,r,l: 96,16,48  v_sync,l,u: 2,10,33 pixclock=251                                                                75000 Hz

imx-ipuv3 2800000.ipu: try ipu internal clk

loop: module loaded

imx-ipuv3 2800000.ipu: disp=0, pixel_clk=25175000 25142857 parent=264000000 div=                                                                10

Wait for CR ACK error!

sata phy RX_PLL is stable!

ahci: SSS flag set, parallel bus scan disabled

ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

scsi0 : ahci_platform

ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71

m25p80 spi32766.0: sst25vf016b (2048 Kbytes)

3 ofpart partitions found on MTD device spi32766.0

Creating 3 MTD partitions on "spi32766.0":

0x000000000000-0x0000000c0000 : "U-Boot"

0x0000000c0000-0x0000000c2000 : "env"

0x0000000c2000-0x000000200000 : "splash"

spi_imx 2008000.ecspi: probed

phyirq=188

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver usbserial_generic

usbserial: USB Serial support registered for generic

usbcore: registered new interface driver cp210x

usbserial: USB Serial support registered for cp210x

usbcore: registered new interface driver ftdi_sio

usbserial: USB Serial support registered for FTDI USB Serial Device

usbcore: registered new interface driver keyspan

usbserial: USB Serial support registered for Keyspan - (without firmware)

usbserial: USB Serial support registered for Keyspan 1 port adapter

usbserial: USB Serial support registered for Keyspan 2 port adapter

usbserial: USB Serial support registered for Keyspan 4 port adapter

usbcore: registered new interface driver pl2303

usbserial: USB Serial support registered for pl2303

usbcore: registered new interface driver qcserial

usbserial: USB Serial support registered for Qualcomm USB modem

setup_reset_gpios:-2

setup_reset_gpios:-2

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

ft5x06-ts 2-0038: ft5x06: Could not detect touch screen.

ft5x06: Jan 27 2016

ili210x_i2c 2-0041: No platform data!

ili210x_i2c 2-0041: i2c transfer failed

ili210x_i2c 2-0041: Failed to get firmware version, err: -5

ili210x_i2c: probe of 2-0041 failed with error -5

setup_reset_gpio:-2

setup_irq_gpio:-2

tsc2004_prepare_for_reading: write_cmd -5

tsc2004: probe of 2-0048 failed with error -5

check_alarm_past: alarm in the past

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

mxc_v4l2_output v4l2_out.36: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.36: V4L2 device registered as video17

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-esdhc-imx 2198000.usdhc: sdhci_esdhc_imx_probe_dt: power-gpio -2

sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on nor                                                                mal mode

mmc0: no vqmmc regulator found

mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

sdhci-esdhc-imx 219c000.usdhc: sdhci_esdhc_imx_probe_dt: power-gpio -2

sdhci-esdhc-imx 219c000.usdhc: could not get ultra high speed state, work on nor                                                                mal mode

mmc1: no vqmmc regulator found

mmc1: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

ata1: SATA link down (SStatus 0 SControl 300)

mmc1: host does not support reading read-only switch. assuming write-enable.

mmc1: new high speed SDHC card at address 0003

mmcblk0: mmc1:0003 SD4GB 3.67 GiB

mmcblk0: p1 p2

mxc_sdc_fb fb.26: 640x480 h_sync,r,l: 96,16,48  v_sync,l,u: 2,10,33 pixclock=252                                                                00000 Hz

imx-ipuv3 2800000.ipu: try ipu internal clk

imx-ipuv3 2800000.ipu: disp=0, pixel_clk=25200000 25142857 parent=264000000 div=                                                                10

usb 1-1: new high-speed USB device number 2 using ci_hdrc

Galcore version 4.6.9.9754

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 3 ports detected

caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)

caam 2100000.caam: job rings = 2, qi = 0

caam 2100000.caam: authenc-hmac-md5-cbc-aes-caam

caam 2100000.caam: authencesn-hmac-md5-cbc-aes-caam

caam 2100000.caam: authenc-hmac-sha1-cbc-aes-caam

caam 2100000.caam: authencesn-hmac-sha1-cbc-aes-caam

caam 2100000.caam: authenc-hmac-sha224-cbc-aes-caam

caam 2100000.caam: authencesn-hmac-sha224-cbc-aes-caam

caam 2100000.caam: authenc-hmac-sha256-cbc-aes-caam

caam 2100000.caam: authencesn-hmac-sha256-cbc-aes-caam

caam 2100000.caam: authenc-hmac-md5-cbc-des3_ede-caam

caam 2100000.caam: authencesn-hmac-md5-cbc-des3_ede-caam

caam 2100000.caam: authenc-hmac-sha1-cbc-des3_ede-caam

caam 2100000.caam: authencesn-hmac-sha1-cbc-des3_ede-caam

caam 2100000.caam: authenc-hmac-sha224-cbc-des3_ede-caam

caam 2100000.caam: authencesn-hmac-sha224-cbc-des3_ede-caam

caam 2100000.caam: authenc-hmac-sha256-cbc-des3_ede-caam

caam 2100000.caam: authencesn-hmac-sha256-cbc-des3_ede-caam

caam 2100000.caam: authenc-hmac-md5-cbc-des-caam

caam 2100000.caam: authencesn-hmac-md5-cbc-des-caam

caam 2100000.caam: authenc-hmac-sha1-cbc-des-caam

caam 2100000.caam: authencesn-hmac-sha1-cbc-des-caam

caam 2100000.caam: authenc-hmac-sha224-cbc-des-caam

caam 2100000.caam: authencesn-hmac-sha224-cbc-des-caam

caam 2100000.caam: authenc-hmac-sha256-cbc-des-caam

caam 2100000.caam: authencesn-hmac-sha256-cbc-des-caam

caam 2100000.caam: ecb-des-caam

caam 2100000.caam: ecb-arc4-caam

caam 2100000.caam: ecb-aes-caam

caam 2100000.caam: ctr-aes-caam

caam 2100000.caam: cbc-aes-caam

caam 2100000.caam: ecb-des3-caam

caam 2100000.caam: cbc-3des-caam

caam 2100000.caam: cbc-des-caam

caam 2100000.caam: fsl,sec-v4.0 algorithms registered in /proc/crypto

platform 2101000.jr0: registering rng-caam

platform caam_sm: caam_sm_test: 8-byte key test match OK

platform caam_sm: caam_sm_test: 16-byte key test match OK

platform caam_sm: caam_sm_test: 32-byte key test match OK

platform caam_secvio.37: security violation service handlers armed

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

sgtl5000 0-000a: sgtl5000 revision 0x11

init_gpio_data:-2

init_gpio_data:-2

sgtl5000 0-000a: Failed to get supply 'VDDD': -19

0-000a: 1200 mV normal

sgtl5000 0-000a: Using internal LDO instead of VDDD

usb 1-1.1: new low-speed USB device number 3 using ci_hdrc

imx-sgtl5000 sound.24:  sgtl5000 <-> 2028000.ssi mapping ok

imx-audio-hdmi sound-hdmi.25:  hdmi-hifi <-> hdmi_audio.16 mapping ok

TCP: cubic registered

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Registering SWP/SWPB emulation handler

input: gpio-keys.23 as /devices/soc0/gpio-keys.23/input/input0

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:01:43 UTC (1                                                                03)

ALSA device list:

  #0: imx6q-sabrelite-sgtl5000

  #1: imx-hdmi-soc

kjournald starting.  Commit interval 5 seconds

EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode

VFS: Mounted root (ext3 filesystem) readonly on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 276K (c0758000 - c079d000)

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.                                                                 See Linux Documentation/init.txt for guidance.

CPU1: stopping

CPU: 1 PID: 0 Comm: swapper/1 Not tainted 3.10.17-1.0.2_ga+yocto+g4da158a #1

Backtrace:

[<c0011da8>] (dump_backtrace+0x0/0x10c) from [<c0011fbc>] (show_stack+0x18/0x1c)

r6:00000000 r5:00000001 r4:c07dbbac r3:00000000

[<c0011fa4>] (show_stack+0x0/0x1c) from [<c0596bb0>] (dump_stack+0x24/0x28)

[<c0596b8c>] (dump_stack+0x0/0x28) from [<c00141e4>] (handle_IPI+0x118/0x134)

[<c00140cc>] (handle_IPI+0x0/0x134) from [<c0008538>] (gic_handle_irq+0x60/0x64)

r6:d208bf00 r5:c07a6904 r4:f400010c r3:00000017

[<c00084d8>] (gic_handle_irq+0x0/0x64) from [<c000e040>] (__irq_svc+0x40/0x50)

Exception stack(0xd208bf00 to 0xd208bf48)

bf00: d208bf48 3b9aca00 9ef1a815 00000000 c07ab85c c1062098 9ef06f95 00000000

bf20: 00000000 00000000 d208a000 d208bf7c 00000002 d208bf48 00000017 c03f4fb8

bf40: 00000113 ffffffff

r7:d208bf34 r6:ffffffff r5:00000113 r4:c03f4fb8

[<c03f4f5c>] (cpuidle_enter_state+0x0/0xec) from [<c03f510c>] (cpuidle_idle_call                                                                +0xc4/0x15c)

r8:c0831fbc r7:c07ab85c r6:00000000 r5:c1062098 r4:00000000

[<c03f5048>] (cpuidle_idle_call+0x0/0x15c) from [<c000f0d4>] (arch_cpu_idle+0x18                                                                /0x54)

[<c000f0bc>] (arch_cpu_idle+0x0/0x54) from [<c005ef8c>] (cpu_startup_entry+0x100                                                                /0x150)

[<c005ee8c>] (cpu_startup_entry+0x0/0x150) from [<c05937ac>] (secondary_start_ke                                                                rnel+0x124/0x130)

r7:c07dbbd8

[<c0593688>] (secondary_start_kernel+0x0/0x130) from [<10592cc4>] (0x10592cc4)

r4:2207806a r3:c0592cac

CPU2: stopping

CPU: 2 PID: 0 Comm: swapper/2 Not tainted 3.10.17-1.0.2_ga+yocto+g4da158a #1

Backtrace:

[<c0011da8>] (dump_backtrace+0x0/0x10c) from [<c0011fbc>] (show_stack+0x18/0x1c)

r6:00000000 r5:00000002 r4:c07dbbac r3:00000000

[<c0011fa4>] (show_stack+0x0/0x1c) from [<c0596bb0>] (dump_stack+0x24/0x28)

[<c0596b8c>] (dump_stack+0x0/0x28) from [<c00141e4>] (handle_IPI+0x118/0x134)

[<c00140cc>] (handle_IPI+0x0/0x134) from [<c0008538>] (gic_handle_irq+0x60/0x64)

r6:d208df00 r5:c07a6904 r4:f400010c r3:00000017

[<c00084d8>] (gic_handle_irq+0x0/0x64) from [<c000e040>] (__irq_svc+0x40/0x50)

Exception stack(0xd208df00 to 0xd208df48)

df00: d208df48 3b9aca00 9ef1a815 00000000 c07ab85c c106a098 9ef07618 00000000

df20: 00000000 00000000 d208c000 d208df7c 00000002 d208df48 00000017 c03f4fb8

df40: 00000113 ffffffff

r7:d208df34 r6:ffffffff r5:00000113 r4:c03f4fb8

[<c03f4f5c>] (cpuidle_enter_state+0x0/0xec) from [<c03f510c>] (cpuidle_idle_call                                                                +0xc4/0x15c)

r8:c0831fbc r7:c07ab85c r6:00000000 r5:c106a098 r4:00000000

[<c03f5048>] (cpuidle_idle_call+0x0/0x15c) from [<c000f0d4>] (arch_cpu_idle+0x18                                                                /0x54)

[<c000f0bc>] (arch_cpu_idle+0x0/0x54) from [<c005ef8c>] (cpu_startup_entry+0x100                                                                /0x150)

[<c005ee8c>] (cpu_startup_entry+0x0/0x150) from [<c05937ac>] (secondary_start_ke                                                                rnel+0x124/0x130)

r7:c07dbbd8

[<c0593688>] (secondary_start_kernel+0x0/0x130) from [<10592cc4>] (0x10592cc4)

r4:2207806a r3:c0592cac

CPU3: stopping

CPU: 3 PID: 133 Comm: kjournald Not tainted 3.10.17-1.0.2_ga+yocto+g4da158a #1

Backtrace:

[<c0011da8>] (dump_backtrace+0x0/0x10c) from [<c0011fbc>] (show_stack+0x18/0x1c)

r6:00000000 r5:00000003 r4:c07dbbac r3:00000000

[<c0011fa4>] (show_stack+0x0/0x1c) from [<c0596bb0>] (dump_stack+0x24/0x28)

[<c0596b8c>] (dump_stack+0x0/0x28) from [<c00141e4>] (handle_IPI+0x118/0x134)

[<c00140cc>] (handle_IPI+0x0/0x134) from [<c0008538>] (gic_handle_irq+0x60/0x64)

r6:d24c7e30 r5:c07a6904 r4:f400010c r3:c0029610

[<c00084d8>] (gic_handle_irq+0x0/0x64) from [<c000e040>] (__irq_svc+0x40/0x50)

Exception stack(0xd24c7e30 to 0xd24c7e78)

7e20:                                     c07dca80 20000193 c07ad13c c07ad13c

7e40: c07dca80 0000002e c07ad134 00000001 00000000 00000000 60000113 d24c7ed4

7e60: d24c7e28 d24c7e78 c0029610 c0029a4c 60000113 ffffffff

r7:d24c7e64 r6:ffffffff r5:60000113 r4:c0029a4c

[<c0029764>] (vprintk_emit+0x0/0x4f8) from [<c0596154>] (printk+0x3c/0x44)

[<c0596118>] (printk+0x0/0x44) from [<c019d704>] (kjournald+0xb8/0x2c4)

r3:000000a0 r2:0000008c r1:00000005 r0:c06c8a10

[<c019d64c>] (kjournald+0x0/0x2c4) from [<c00478e8>] (kthread+0xbc/0xc0)

[<c004782c>] (kthread+0x0/0xc0) from [<c000e4d8>] (ret_from_fork+0x14/0x3c)

r7:00000000 r6:00000000 r5:c004782c r4:d2069c40

Regards

Senthil

0 件の賞賛
返信