Anyone seen a compact iMX6 eval board with easy access to I2S?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone seen a compact iMX6 eval board with easy access to I2S?

662 Views
EdSutter
Senior Contributor II

I may be involved in a project that needs to hook up the iMX6 to a different audio chip (seems like most eval boards are using the same Freescale codec).

I thought it would be a common access point on the (many) eval board headers; however after looking at two or three I'm seeing that most just provide audio jacks and use their own codec (no direct I2S access).  Has anyone seen a compact imx6 eval board that allows me to hook up to its I2S bus?

Tx

Tags (2)
0 Kudos
2 Replies

403 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ed

seems one can look at i.MX6 Wandboards, like

http://www.wandboard.org/images/downloads/wbquad-revb1-userguide.pdf

p.23, signals AUD3_* on J1B (MXM_3.0_CONNECTOR-X/281+E40)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

403 Views
EdSutter
Senior Contributor II

Igor,

Thanks for responding...

Yea, I'm aware of that connection point (I've played with a wandboard).

Unfortunately J1 is the main connector between the CPU module and

the carrier board, so there's no clean physical access to this on the carrier board

(at least not that I've discovered).  I'm trying to avoid hacking the board if

possible; however, as my search continues, it may turn out that I have no

choice!

Thanks!

Ed

0 Kudos