Any suggestion on VNC server for android lollipop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any suggestion on VNC server for android lollipop

2,354件の閲覧回数
damienhuang
Contributor IV

Hi,

I would like to control my android tablet that has lollipop 5.0.2 installed over Ethernet with VNC

Any good VNC server can be suggested?

Cheers,

Damien

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,003件の閲覧回数
b36401
NXP Employee
NXP Employee

You can run VNC server with the command like this on your board:
# /usr/bin/x11vnc -display :smileylaugh:

Then you will see such lines among the diasnostics:

The VNC desktop is: imx6qdlsolo:0
PORT=5900

These lines mean that it is #0 X sevrer on the host.

And then you can use any of VNC clients to access your VNC server:

https://help.ubuntu.com/community/VNC/Clients

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,003件の閲覧回数
damienhuang
Contributor IV

Sorry Victor, I am a bit confused.

I am using Android Lollipop 5.02, and I can no find "/usr/bin" directory.

Cheers,

Damien

0 件の賞賛
返信