Hi Support,
We found the performance of SPI interface is about TX 4.2Mbps, RX 3.6Mbps. Do you know any buffer in cspi that we can enlarge to see any improvement, especially RX path ?
Regards,
Steven Yu
Hi Steven
for eCSPI module one can try to increase BURST_LENGTH parameter
in ECSPIx_CONREG register. For processors with M4 core one can assign
spi procedures to this core. In general spi performance will depend on processor
load and application.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks, igor!
We have seen this piece of code in static spi_imx_setupxfer, however, if we double the value, it will cause spi read data error.
if (bits == 32) {
 unsigned len = spi_imx->len / 4;
 
 while (len > 128) {
 if (len & 1)
 break;
 len >>= 1;
 }
 while (len > 128) {
 if (len % 3)
 break;
 len /= 3;
 }
 if ((len > 128) || !len)
 len = 1;
 bits = len << 5;
 }
 ctrl |= (bits - 1) << MX51_ECSPI_CTRL_BL_OFFSET;
==>
ctrl |= (2*(bits - 1)) << MX51_ECSPI_CTRL_BL_OFFSET;
Regards,
Steven Yu