Android9: qca9377 BT speed issue on IMX8M-Mini platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android9: qca9377 BT speed issue on IMX8M-Mini platform

1,628 次查看
mayqueen
Contributor IV

Hello:

Platform: IMX8M-Mini

OS: Android 9 (p9.0.0-1.0.0_ga bsp)

WiFi module: QCA9377

Issue description:

basically, the bluetooth works fine but the speed is fixed on 115200bps, I already tweaked the HAL layer (hardware/qcom/bt/) and force to config the uart baud rate as 3Mbps as following link, but still the same results.

I also trying to change firmware and modify serial driver of linux kernel but no any improvement...Do you know how to improve it or recommend suitable people to me, I need helps with directions.

Thanks

0 项奖励
回复
1 回复

1,417 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello May,

Unfortunately!  band rate has been fixed in firmware, which can't be changed.

Have a nice day!

Best regards,

NXP TIC team Weidong

0 项奖励
回复