Hi NXP team:
I need OTA function in imx6q-sabresd.
When I input the command as below:
sabresd_6dq:/ #
sabresd_6dq:/ #
sabresd_6dq:/ #
sabresd_6dq:/ # reboot recovery
sysrq: SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command 'recovery'
U-Boot 2015.04-00001-g9f38145-dirty (Apr 22 2019 - 10:07:10)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 59 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:2
Fastboot: Normal -----------------------why there is Normal but not recovery
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.
But it can not enter recovery mode,it boot up normally .
Could anyone tell me how to change it ?