We found Android4.4 KitKat by the following URL.
<URL>
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/
- kk4.4.2_1.0.0-alpha
We would like to implement it to MCIMX6DL_SABRE-SDP.
However, when building, an error occurs in installation of a patch.
Is there any information for building this?
May I have advice?
Best Regards,
已解决! 转到解答。
This is internal release of Linux kernel.
You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.
Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.
This is internal release of Linux kernel.
You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.
Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.