Android4.4 kitkat for i.MX6DL SABRE-SDP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android4.4 kitkat for i.MX6DL SABRE-SDP

ソリューションへジャンプ
1,498件の閲覧回数
yuuki
Senior Contributor II

We found Android4.4 KitKat by the following URL.

<URL>
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/
- kk4.4.2_1.0.0-alpha

We would like to implement it to MCIMX6DL_SABRE-SDP.

However, when building, an error occurs in installation of a patch.

Is there any information for building this?
May I have advice?

Best Regards,

ラベル(1)
タグ(4)
1 解決策
501件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

This is internal release of Linux kernel.

You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.

Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.

元の投稿で解決策を見る

1 返信
502件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

This is internal release of Linux kernel.

You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.

Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.