Android4.4 kitkat for i.MX6DL SABRE-SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android4.4 kitkat for i.MX6DL SABRE-SDP

Jump to solution
1,501 Views
yuuki
Senior Contributor II

We found Android4.4 KitKat by the following URL.

<URL>
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/
- kk4.4.2_1.0.0-alpha

We would like to implement it to MCIMX6DL_SABRE-SDP.

However, when building, an error occurs in installation of a patch.

Is there any information for building this?
May I have advice?

Best Regards,

Labels (1)
1 Solution
504 Views
justin_jiang
NXP Employee
NXP Employee

This is internal release of Linux kernel.

You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.

Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.

View solution in original post

1 Reply
505 Views
justin_jiang
NXP Employee
NXP Employee

This is internal release of Linux kernel.

You can waiting for the KK4.4.2_1.0.0GA release and build the Kernel with Android together.

Currently, if you want to build the kernel only, you can try to use Freescale cross-compiler.