Android upgrade through recovery.img

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android upgrade through recovery.img

跳至解决方案
13,365 次查看
ashishgupta
Contributor III

Hi All,

I am trying to use recovery.img for upgrading android images (boot.img, system.img, recovery.img) in eMMC Nand  flash. Please suggest if it is feasible to hack recovery.img to automate the upgrade process. Please provide any link or document in this regard.

Problem while using recovery.img

========================

When i boot sabresd board in recovery mode (by pressing vol-down button) from eMMC, the boot up process hangs at "Freeing init memory" and android recovery icon appears on hdmi display. The same image boots up properly in normal mode with the bootargs=console=ttymxc0,115200 androidboot.console=ttymxc0 init=/init vmalloc=400M video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=28M androidboot.hardware=freescale.

Thanks & Regards,

Ashish Gupta

标签 (3)
0 项奖励
回复
1 解答
7,193 次查看
raymondwang
Senior Contributor I

Yes,they are different.

1.If you want to building updatepackage for fastboot.

$make updatepackage

THis is just a zip file including target board binary images (boot.img,recovery.img,system.img)

You can use it in fastboot mode.

$fastboot update yourupdatepackage.zip  --this will check target board name

2.Well,the otapackage is a zip file including your whole target system files Generally otapackage building require

device key.Of course you can use fsl common device key in device/fsl/common/security and this is default setting in BoardConfig.mk

by below lines:

PRODUCT_DEFAULT_DEV_CERTIFICATE := \

        device/fsl/common/security/testkey

  Here I list my otapackage zip file dir:

  boot.img

  system/   --including all your system files like your out/target/product/xxx/system

  recovery/  --including recovery script and recovery.P

  META-INF/  --including script and CERT,signature of your ota package which is used by recovery image.

在原帖中查看解决方案

0 项奖励
回复
7 回复数
7,192 次查看
ashishgupta
Contributor III

Hi Raymond,

After rebuilding the android source JB422, i am able to generate OTA package "sabresd_6dq-ota-eng.root.zip". And this file has same directory list as you have mentioned.

I rename this file to update.zip and copied it to sabresd cache folder. My sabresd board is running Android 13.4.1 (4.0.0) image and i am doing a POC which will upgrade it to JB422 through this OTA package.

After copying it to cache folder, i made command file in recovery folder, with following:

--update_package=/cache/update.zip

and restarted the system in recovery mode. On HDMI display i am able to see the Android Robot while upgrading and after upgrading it prints successful message in the display.

But when i restart the system, it keeps on rebooting after loading the kernel. Please suggest.

Thanks & Regards,

Ashish Gupta

0 项奖励
回复
7,193 次查看
raymondwang
Senior Contributor I

Android recovery only provide mechanism of updating your system. After upgrading completed,it will reboot automatically.

If your board always restart after kernel is loading, you should check your boot.img and system.img.

For example,you can upgrade your kernel (boot.img=kernel+ramdisk) and system.img by fastboot

in device uboot console

$fastboot

in your usb otg connected linux machine(We assume you have permission to access adb devices)

$fastboot flash boot out/target/product/XXX/boot.img

$fastboot flash system out/target/product/XXX/system.img

$fastboot reboot

As a summary,you should check your boot.img and system.img can boot up properly. They are nothing to do with android

recovery OTA .

0 项奖励
回复
7,193 次查看
ashishgupta
Contributor III

Hi Raymond wang,

Ofcourse you answer is helpful, but i am stuck little bit while generating the OTA package.

Today i tried to build the ota package based on the instructions mentioned in 13.4.1 "Android_Advanced_User_Guide.pdf".

After,

$ make PRODUCT=sabresd_6dq-eng dist -j4

I can find out/dist/ folder and following zip files inside:

-rw-r--r-- 1 root root  53284796 Nov  7 12:28 full-apps-eng.root.zip
-rw-r--r-- 1 root root 121056186 Nov  7 12:29 full-emulator-eng.root.zip
-rw-r--r-- 1 root root 564312424 Nov  7 12:30 full-symbols-eng.root.zip
-rw-r--r-- 1 root root 118854623 Nov  7 12:29 full-target_files-eng.root.zip

And no zip file is created in the out/target/product/sabresd_6q/

Then i tried to update the board with fastboot

$ fastboot update full-target_files-eng.root.zip

But it is failing.

Also $ make otapackage, does'nt work.

Ques: Whether update.zip is the same file as full-target_files-eng.root.zip? Or there is a different command for generating update.zip?

b.t.w. i am using jb4.2.2_1_0_0 patches for compiling android, and have sabresd imx6q board.

0 项奖励
回复
7,194 次查看
raymondwang
Senior Contributor I

Yes,they are different.

1.If you want to building updatepackage for fastboot.

$make updatepackage

THis is just a zip file including target board binary images (boot.img,recovery.img,system.img)

You can use it in fastboot mode.

$fastboot update yourupdatepackage.zip  --this will check target board name

2.Well,the otapackage is a zip file including your whole target system files Generally otapackage building require

device key.Of course you can use fsl common device key in device/fsl/common/security and this is default setting in BoardConfig.mk

by below lines:

PRODUCT_DEFAULT_DEV_CERTIFICATE := \

        device/fsl/common/security/testkey

  Here I list my otapackage zip file dir:

  boot.img

  system/   --including all your system files like your out/target/product/xxx/system

  recovery/  --including recovery script and recovery.P

  META-INF/  --including script and CERT,signature of your ota package which is used by recovery image.

0 项奖励
回复
7,193 次查看
raymondwang
Senior Contributor I

Recovery.img boot without console in default so it seems system hangup in console.

You can test ota package with your recovery.img

Step 1: building otapackage

$make otapackage

Step 2:

$adb push update.zip /cache  #assume update.zip is your otapackage

$adb shell

#Now in device shell

#mkdir /cache/recovery/

#echo "--update_package=/cache/update.zip" > /cache/recovery/command

#reboot recovery


Now your android will reboot to recovery mode to update your OTA package,it will reboot automatically after finished.

7,193 次查看
ashishgupta
Contributor III

Thanks Raymond Wang, for the guiding us in the right direction.

0 项奖励
回复
7,193 次查看
raymondwang
Senior Contributor I

If your problem resolved,please mark thread as answered or help answered.

0 项奖励
回复