Android or other Linux on the UL, where to start?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android or other Linux on the UL, where to start?

879 次查看
claudiohediger
Contributor I

Hi

We have here an i.MX6UL EVK with Display.

We would like to use any kind of Linuxdistribution on it to run our own application.

In the end, the Board should be able to play audiofiles from an SD-Card with our own GUI.

Can anyone tell us, where we can start?

Thanks :smileyhappy:

标签 (1)
0 项奖励
回复
1 回复

752 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Claudio

linux is more simple, suggest to start with

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul) New

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复