Android or other Linux on the UL, where to start?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android or other Linux on the UL, where to start?

896件の閲覧回数
claudiohediger
Contributor I

Hi

We have here an i.MX6UL EVK with Display.

We would like to use any kind of Linuxdistribution on it to run our own application.

In the end, the Board should be able to play audiofiles from an SD-Card with our own GUI.

Can anyone tell us, where we can start?

Thanks :smileyhappy:

ラベル(1)
0 件の賞賛
返信
1 返信

769件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Claudio

linux is more simple, suggest to start with

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul) New

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信