Android kernel not booting on iMX8MP platform, instead it shuts down.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android kernel not booting on iMX8MP platform, instead it shuts down.

2,571 次查看
swapnilpendhare
Contributor III

I am trying to port Android 11.0.2.6.0 on imx8MP based EVK board developed by Compulab. 
the board name is ucm-imx8m-plus evk board.

When i am trying to boot kernel i am getting following mesg and kernel reboots. What could be the problem. 


U-Boot SPL 2021.04-00001-g302084ead7-dirty (May 10 2022 - 02:16:02 +0530)
DDRINFO: Cfg attempt: [ 3/4 ]
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
DDRINFO(M): mr5-8 [ 0xff000010 ]
DDRINFO(T): mr5-8 [ 0xff000010 ]
DDRINFO(E): mr5-8 [ 0xff000010 ], read back
spl_dram_init Continue w/out reset ...
Normal Boot
WDT: Not starting
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Failed to find node!, err: -1!
Failed to find node!, err: -1!
NOTICE: BL31: v2.4(release):android-11.0.0_2.6.0-0-g2ff011d64
NOTICE: BL31: Built : 02:16:55, May 10 2022


U-Boot 2021.04-00001-g302084ead7-dirty (May 10 2022 - 02:16:02 +0530)

CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 53C
Reset cause: POR
Model: CompuLab UCM-iMX8M-Plus
DRAM: 4 GiB
WDT: Started with servicing (60s timeout)
MMC: FSL_SDHC: 1, FSL_SDHC: 2
[*]-Video Link 0 (720 x 1280)
[0] lcd-controller@32e80000, video
[1] mipi_dsi@32e60000, video_bridge
[2] ili9881c_panel, panel
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 2ff011d

flash target is MMC:1
Net: eth1: ethernet@30bf0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Writing A/B metadata to disk.
verify OK, boot 'boot_a'
Kernel load addr 0x40480000 size 33843 KiB
kernel @ 40480000 (35782656)
ramdisk @ 44680000 (14598036)
fdt @ 42820400 (64433)
Moving Image from 0x40480000 to 0x40600000, end=42820000
## Flattened Device Tree blob at 42820400
Booting using the fdt blob at 0x42820400
Using Device Tree in place at 0000000042820400, end 0000000042832fb0

Starting kernel ...

[ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000][ T0] Linux version 5.10.72-00001-gcb6f328b5e81-dirty (swapnil@AGLPUN-D0322U) (Android (7284624, based on r416183b) clang version 12.0.5 (https://android.googlesource.com/toolchain/llvm-project c935d99d7cf2016289302412d708641d52d2f7ee), LLD 12.0.5 (/buildbot/src/android/llvm-toolchain/out/llvm-project/lld c935d99d7cf2016289302412d708641d52d2f7ee)) #16 SMP PREEMPT Tue May 10 00:00:56 IST 2022
[ 0.000000][ T0] Machine model: CompuLab UCM-iMX8M-Plus
[ 0.000000][ T0] Stack Depot is disabled
[ 0.000000][ T0] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000][ T0] printk: bootconsole [ec_imx6q0] enabled
[ 0.000000][ T0] efi: UEFI not found.
[ 0.000000][ T0] Reserved memory: bypass linux,cma node, using cmdline CMA params instead
[ 0.000000][ T0] OF: reserved mem: node linux,cma compatible matching fail
[ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[ 0.000000][ T0] NUMA: No NUMA configuration found
[ 0.000000][ T0] NUMA: Faking a node at [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] NUMA: NODE_DATA [mem 0x13f844000-0x13f845fff]
[ 0.000000][ T0] kvm [0]: Reserved 22 MiB at 0x13e200000
[ 0.000000][ T0] Zone ranges:
[ 0.000000][ T0] DMA32 [mem 0x0000000040000000-0x00000000ffffffff]
[ 0.000000][ T0] Normal [mem 0x0000000100000000-0x000000013fffffff]
[ 0.000000][ T0] Movable zone start for each node
[ 0.000000][ T0] Early memory node ranges
[ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000557fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000055800000-0x0000000055ffffff]
[ 0.000000][ T0] node 0: [mem 0x0000000056000000-0x00000000823fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000082400000-0x00000000943fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094400000-0x00000000944fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094500000-0x000000009450ffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094510000-0x000000013fffffff]
[ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] cma: Reserved 960 MiB at 0x00000000a4000000
[ 0.000000][ T0] psci: probing for conduit method from DT.
[ 0.000000][ T0] psci: PSCIv1.1 detected in firmware.
[ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs
[ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000][ T0] psci: SMC Calling Convention v1.2
[ 0.000000][ T0] percpu: Embedded 24 pages/cpu s60888 r8192 d29224 u98304
[ 0.000000][ T0] Detected VIPT I-cache on CPU0
[ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[ 0.000000][ T0] CPU features: detected: ARM erratum 845719
[ 0.000000][ T0] CPU features: detected: GIC system register CPU interface
[ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000][ T0] Policy zone: Normal
[ 0.000000][ T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure cgroup.memory=nokmem console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 console=tty0 init=/init androidboot.console=ttymxc1 androidboot.hardware=nxp firmware_class.path=/vendor/firmware loop.max_part=7 transparent_hugepage=never swiotlb=65536 androidboot.lcd_density=240 androidboot.primary_display=imx-drm cma=960M@0x400M-0x1000M androidboot.vendor.sysrq=1 buildvariant=userdebug androidboot.serialno=062040000882277a androidboot.btmacaddr=06:20:40:00:08:82 androidboot.soc_type=imx8mp androidboot.boot_device_root=mmcblk1 androidboot.boottime=1BLL:0,1BLE:7302,KL:0,KD:0,AVB:3529,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.dtbo_idx=0 androidboot.keystore=software androidboot.verifiedbootstate=green androidboot.flash.locked=1 androidboot.slot_suffix=_a androidboot.vbmeta.device=PARTUUID=ad685e6f-a2a1-4067-9240-cedd281c90f0 androidbo
[ 0.000000][ T0] cgroup: Disabling pressure control group feature
[ 0.000000][ T0] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000][ T0] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000][ T0] mem auto-init: stack:off, heap alloc:on, heap free:off
[ 0.000000][ T0] software IO TLB: mapped [mem 0x00000000f7fff000-0x00000000fffff000] (128MB)
[ 0.000000][ T0] Memory: 2360660K/4194304K available (19328K kernel code, 1586K rwdata, 11496K rodata, 1280K init, 1068K bss, 850604K reserved, 983040K cma-reserved)
[ 0.000000][ T0] random: get_random_u64 called from kmem_cache_open+0x30/0x3c8 with crng_init=0
[ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000][ T0] rcu: RCU event tracing is enabled.
[ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[ 0.000000][ T0] Trampoline variant of Tasks RCU enabled.
[ 0.000000][ T0] Tracing variant of Tasks RCU enabled.
[ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000][ T0] GICv3: 160 SPIs implemented
[ 0.000000][ T0] GICv3: 0 Extended SPIs implemented
[ 0.000000][ T0] GICv3: Distributor has no Range Selector support
[ 0.000000][ T0] GICv3: 16 PPIs implemented
[ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000][ T0] ITS: No ITS available, not enabling LPIs
[ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none).
[ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000004][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.009704][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.019784][ T0] pid_max: default: 32768 minimum: 301
[ 0.025228][ T0] LSM: Security Framework initializing
[ 0.030498][ T0] SELinux: Initializing.
[ 0.034800][ T0] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.042803][ T0] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.053175][ T1] rcu: Hierarchical SRCU implementation.
[ 0.058525][ T1] EFI services will not be available.
[ 0.062377][ T1] smp: Bringing up secondary CPUs ...
[ 0.067896][ T0] Detected VIPT I-cache on CPU1
[ 0.067919][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.067955][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.068501][ T0] Detected VIPT I-cache on CPU2
[ 0.068518][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.068539][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.069059][ T0] Detected VIPT I-cache on CPU3
[ 0.069074][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.069094][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.069167][ T1] smp: Brought up 1 node, 4 CPUs
[ 0.131007][ T1] SMP: Total of 4 processors activated.
[ 0.136421][ T1] CPU features: detected: 32-bit EL0 Support
[ 0.142300][ T1] CPU features: detected: CRC32 instructions
[ 0.148148][ T1] CPU features: detected: 32-bit EL1 Support
[ 0.154019][ T1] CPU features: detected: Protected KVM
[ 0.159491][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.181417][ T1] CPU: All CPU(s) started at EL2
[ 0.183385][ T14] alternatives: patching kernel code
[ 0.190255][ T1] devtmpfs: initialized
[ 0.205313][ T1] Registered cp15_barrier emulation handler
[ 0.208237][ T1] Registered setend emulation handler
[ 0.213487][ T1] KASLR disabled due to lack of seed
[ 0.218807][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.229160][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.286796][ T1] pinctrl core: initialized pinctrl subsystem
[ 0.290985][ T1] NET: Registered protocol family 16
[ 0.309849][ T1] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.316397][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.323595][ T1] audit: initializing netlink subsys (disabled)
[ 0.329821][ T37] audit: type=2000 audit(0.240:1): state=initialized audit_enabled=0 res=1
[ 0.330508][ T1] thermal_sys: Registered thermal governor 'step_wise'
[ 0.338063][ T1] thermal_sys: Registered thermal governor 'user_space'
[ 0.344794][ T1] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.351968][ T1] cpuidle: using governor menu
[ 0.364171][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.371128][ T1] ASID allocator initialised with 65536 entries
[ 0.378278][ T1] Serial: AMBA PL011 UART driver
[ 0.382060][ T1] imx rpmsg driver is registered.
[ 0.387770][ T1] printk: console [ramoops-1] enabled
[ 0.392344][ T1] pstore: Registered ramoops as persistent store backend
[ 0.399050][ T1] ramoops: using 0x100000@0x94400000, ecc: 0
[ 0.462695][ T1] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.467319][ T1] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.474720][ T1] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.482154][ T1] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.494921][ T1] ACPI: Interpreter disabled.
[ 0.497733][ T1] iommu: Default domain type: Translated
[ 0.502841][ T1] SCSI subsystem initialized
[ 0.507003][ T1] usbcore: registered new interface driver usbfs
[ 0.512938][ T1] usbcore: registered new interface driver hub
[ 0.518966][ T1] usbcore: registered new device driver usb
[ 0.525453][ T1] mc: Linux media interface: v0.10
[ 0.529715][ T1] videodev: Linux video capture interface: v2.00
[ 0.536001][ T1] pps_core: LinuxPPS API ver. 1 registered
[ 0.541593][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.551498][ T1] PTP clock support registered
[ 0.556323][ T1] EDAC MC: Ver: 3.0.0
[ 0.561332][ T1] FPGA manager framework
[ 0.564183][ T1] Advanced Linux Sound Architecture Driver Initialized.
[ 0.571592][ T1] nfc: nfc_init: NFC Core ver 0.1
[ 0.575848][ T1] NET: Registered protocol family 39
[ 0.582417][ T1] clocksource: Switched to clocksource arch_sys_counter
[ 0.588038][ T1] VFS: Disk quotas dquot_6.6.0
[ 0.592475][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.600249][ T1] pnp: PnP ACPI: disabled
[ 0.605877][ T1] NET: Registered protocol family 2
[ 0.609465][ T1] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.619175][ T1] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.626858][ T1] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.635681][ T1] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.643906][ T1] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.650841][ T1] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.658233][ T1] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.666211][ T1] NET: Registered protocol family 1
[ 0.671113][ T1] NET: Registered protocol family 44
[ 0.676263][ T1] PCI: CLS 0 bytes, default 64
[ 0.681113][ T1] Trying to unpack rootfs image as initramfs...
[ 1.330673][ T1] Freeing initrd memory: 14252K
[ 1.333675][ T1] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.341758][ T1] kvm [1]: IPA Size Limit: 40 bits
[ 1.365577][ T1] kvm [1]: GICv3: no GICV resource entry
[ 1.368241][ T1] kvm [1]: disabling GICv2 emulation
[ 1.373409][ T1] kvm [1]: GIC system register CPU interface enabled
[ 1.380079][ T1] kvm [1]: vgic interrupt IRQ9
[ 1.385127][ T1] kvm [1]: Protected nVHE mode initialized successfully
[ 1.397231][ T1] Initialise system trusted keyrings
[ 1.399817][ T1] workingset: timestamp_bits=42 max_order=20 bucket_order=0
[ 1.417863][ T1] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.421892][ T1] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.429252][ T1] fuse: init (API version 7.32)
[ 1.433525][ T1] 9p: Installing v9fs 9p2000 file system support
[ 1.474941][ T1] Key type asymmetric registered
[ 1.476899][ T1] Asymmetric key parser 'x509' registered
[ 1.482555][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 236)
[ 1.490666][ T1] io scheduler mq-deadline registered
[ 1.495906][ T1] io scheduler kyber registered
[ 1.500763][ T1] io scheduler bfq registered
[ 1.512291][ T1] EINJ: ACPI disabled.
[ 1.517175][ T1] SoC: i.MX8MP revision 1.1
[ 1.521886][ T1] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.538352][ T1] brd: module loaded
[ 1.550616][ T1] loop: module loaded
[ 1.553355][ T7] nd_pmem namespace0.0: unable to guarantee persistence of writes
[ 1.554023][ T1] megasas: 07.714.04.00-rc1
[ 1.566311][ T1] imx ahci driver is registered.
[ 1.572962][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
[ 1.578690][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 1.590399][ T1] libphy: Fixed MDIO Bus: probed
[ 1.595255][ T1] tun: Universal TUN/TAP device driver, 1.6
[ 1.599795][ T1] CAN device driver interface
[ 1.605021][ T1] thunder_xcv, ver 1.0
[ 1.608121][ T1] thunder_bgx, ver 1.0
[ 1.612058][ T1] nicpf, ver 1.0
[ 1.617135][ T1] hclge is initializing
[ 1.619478][ T1] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.627419][ T1] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.633512][ T1] e1000: Intel(R) PRO/1000 Network Driver
[ 1.639058][ T1] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.645570][ T1] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.651218][ T1] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.657930][ T1] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.664002][ T1] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.670374][ T1] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.677295][ T1] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.684165][ T1] sky2: driver version 1.30
[ 1.689686][ T1] PPP generic driver version 2.4.2
[ 1.693450][ T1] PPP BSD Compression module registered
[ 1.698739][ T1] PPP Deflate Compression module registered
[ 1.704527][ T1] PPP MPPE Compression module registered
[ 1.710021][ T1] NET: Registered protocol family 24
[ 1.715181][ T1] PPTP driver version 0.8.5
[ 1.720037][ T1] VFIO - User Level meta-driver version: 0.3
[ 1.728427][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.732840][ T1] ehci-pci: EHCI PCI platform driver
[ 1.738036][ T1] ehci-platform: EHCI generic platform driver
[ 1.744220][ T1] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.750879][ T1] ohci-pci: OHCI PCI platform driver
[ 1.756057][ T1] ohci-platform: OHCI generic platform driver
[ 1.762861][ T1] usbcore: registered new interface driver cdc_acm
[ 1.768360][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.777279][ T1] usbcore: registered new interface driver uas
[ 1.783206][ T1] usbcore: registered new interface driver usb-storage
[ 1.789958][ T1] usbcore: registered new interface driver usbserial_generic
[ 1.797165][ T1] usbserial: USB Serial support registered for generic
[ 1.803915][ T1] usbcore: registered new interface driver ftdi_sio
[ 1.810375][ T1] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.818470][ T1] usbcore: registered new interface driver usb_serial_simple
[ 1.825686][ T1] usbserial: USB Serial support registered for carelink
[ 1.832517][ T1] usbserial: USB Serial support registered for zio
[ 1.838902][ T1] usbserial: USB Serial support registered for funsoft
[ 1.845636][ T1] usbserial: USB Serial support registered for flashloader
[ 1.852727][ T1] usbserial: USB Serial support registered for google
[ 1.859375][ T1] usbserial: USB Serial support registered for libtransistor
[ 1.866644][ T1] usbserial: USB Serial support registered for vivopay
[ 1.873375][ T1] usbserial: USB Serial support registered for moto_modem
[ 1.880375][ T1] usbserial: USB Serial support registered for motorola_tetra
[ 1.887765][ T1] usbserial: USB Serial support registered for novatel_gps
[ 1.894812][ T1] usbserial: USB Serial support registered for hp4x
[ 1.901286][ T1] usbserial: USB Serial support registered for suunto
[ 1.907952][ T1] usbserial: USB Serial support registered for siemens_mpi
[ 1.915045][ T1] usbcore: registered new interface driver usb_ehset_test
[ 1.922844][ T1] dummy_hcd dummy_hcd.0: USB Host+Gadget Emulator, driver 02 May 2005
[ 1.930071][ T1] dummy_hcd dummy_hcd.0: Dummy host controller
[ 1.936101][ T1] dummy_hcd dummy_hcd.0: new USB bus registered, assigned bus number 1
[ 1.944400][ T1] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 1.953249][ T1] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.961211][ T1] usb usb1: Product: Dummy host controller
[ 1.966898][ T1] usb usb1: Manufacturer: Linux 5.10.72-00001-gcb6f328b5e81-dirty dummy_hcd
[ 1.975470][ T1] usb usb1: SerialNumber: dummy_hcd.0
[ 1.981135][ T1] hub 1-0:1.0: USB hub found
[ 1.985212][ T1] hub 1-0:1.0: 1 port detected
[ 1.991549][ T1] usbcore: registered new interface driver xpad
[ 1.997131][ T1] i2c /dev entries driver
[ 2.001090][ T1] usbcore: registered new interface driver uvcvideo
[ 2.006625][ T1] USB Video Class driver (1.1.1)
[ 2.011432][ T1] gspca_main: v2.14.0 registered
[ 2.018172][ T1] device-mapper: uevent: version 1.0.3
[ 2.021910][ T1] device-mapper: ioctl: 4.44.0-ioctl (2021-02-01) initialised: dm-devel@redhat.com
[ 2.031425][ T1] EDAC MC: ECC not enabled
[ 2.036251][ T1] sdhci: Secure Digital Host Controller Interface driver
[ 2.041983][ T1] sdhci: Copyright(c) Pierre Ossman
[ 2.047559][ T1] Synopsys Designware Multimedia Card Interface Driver
[ 2.054641][ T1] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.061830][ T1] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.067129][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 2.074130][ T1] hid: raw HID events driver (C) Jiri Kosina
[ 2.081775][ T1] usbcore: registered new interface driver usbhid
[ 2.086251][ T1] usbhid: USB HID core driver
[ 2.092172][ T1] ashmem: initialized
[ 2.098843][ T1] gnss: GNSS driver registered with major 502
[ 2.104908][ T1] NET: Registered protocol family 26
[ 2.107255][ T1] GACT probability NOT on
[ 2.111422][ T1] Mirror/redirect action on
[ 2.115800][ T1] netem: version 1.3
[ 2.119645][ T1] u32 classifier
[ 2.122966][ T1] input device check on
[ 2.127339][ T1] Actions configured
[ 2.132396][ T1] xt_time: kernel timezone is -0000
[ 2.136706][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 2.143133][ T1] gre: GRE over IPv4 demultiplexor driver
[ 2.148345][ T1] ip_gre: GRE over IPv4 tunneling driver
[ 2.154813][ T1] IPv4 over IPsec tunneling driver
[ 2.159459][ T1] Initializing XFRM netlink socket
[ 2.163863][ T1] IPsec XFRM device driver
[ 2.168678][ T1] NET: Registered protocol family 10
[ 2.175103][ T1] Segment Routing with IPv6
[ 2.177799][ T1] mip6: Mobile IPv6
[ 2.182598][ T1] ip6_gre: GRE over IPv6 tunneling driver
[ 2.187401][ T1] NET: Registered protocol family 17
[ 2.192143][ T1] NET: Registered protocol family 15
[ 2.197399][ T1] can: controller area network core
[ 2.202496][ T1] NET: Registered protocol family 29
[ 2.207500][ T1] can: raw protocol
[ 2.211191][ T1] can: broadcast manager protocol
[ 2.216082][ T1] can: netlink gateway - max_hops=1
[ 2.221255][ T1] l2tp_core: L2TP core driver, V2.0
[ 2.226222][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.231728][ T1] tipc: Activated (version 2.0.0)
[ 2.236831][ T1] NET: Registered protocol family 30
[ 2.242016][ T1] tipc: Started in single node mode
[ 2.246997][ T1] 9pnet: Installing 9P2000 support
[ 2.257123][ T1] NET: Registered protocol family 36
[ 2.259833][ T1] NET: Registered protocol family 40
[ 2.265509][ T1] registered taskstats version 1
[ 2.269438][ T1] Loading compiled-in X.509 certificates
[ 2.274989][ T1] page_owner is disabled
[ 2.279178][ T1] Key type ._fscrypt registered
[ 2.283759][ T1] Key type .fscrypt registered
[ 2.288401][ T1] Key type fscrypt-provisioning registered
[ 2.295132][ T1] pstore: Using crash dump compression: deflate
[ 2.306164][ T1] ALSA device list:
[ 2.307012][ T1] No soundcards found.
[ 2.311142][ T1] Warning: unable to open an initial console.
[ 2.318741][ T1] Freeing unused kernel memory: 1280K
[ 2.338495][ T1] Run /init as init process
[ 2.375342][ T1] init: init first stage started!
[ 2.382612][ T1] init: alias lines in modules.alias must have 3 entries, not 4
[ 2.388132][ T1] init: alias lines in modules.alias must have 3 entries, not 4
[ 2.397925][ T1] init: alias lines in modules.alias must have 3 entries, not 4
[ 2.406324][ T1] init: alias lines in modules.alias must have 3 entries, not 4
[ 2.417361][ T1] init: Loading module /lib/modules/synaptics_dsx_i2c.ko with args ""
[ 2.424467][ T1] init: Loaded kernel module /lib/modules/synaptics_dsx_i2c.ko
[ 2.430721][ T1] init: Loading module /lib/modules/cfg80211.ko with args ""
[ 2.445850][ T1] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.452689][ T142] random: sh: uninitialized urandom read (40 bytes read)
[ 2.460791][ T142] random: sh: uninitialized urandom read (40 bytes read)
[ 2.465533][ T142] random: sh: uninitialized urandom read (4 bytes read)
[ 2.481553][ T1] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.486090][ T33] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.491139][ T1] init: Loaded kernel module /lib/modules/cfg80211.ko
[ 2.495348][ T33] cfg80211: failed to load regulatory.db
[ 2.502672][ T1] init: Loading module /lib/modules/libdes.ko with args ""
[ 2.582461][ T1] raid6: neonx8 gen() 2260 MB/s
[ 2.650718][ T1] raid6: neonx8 xor() 1671 MB/s
[ 2.718424][ T1] raid6: neonx4 gen() 2158 MB/s
[ 2.786415][ T1] raid6: neonx4 xor() 1551 MB/s
[ 2.854423][ T1] raid6: neonx2 gen() 2018 MB/s
[ 2.922413][ T1] raid6: neonx2 xor() 1454 MB/s
[ 2.990439][ T1] raid6: neonx1 gen() 1710 MB/s
[ 3.058439][ T1] raid6: neonx1 xor() 1244 MB/s
[ 3.126737][ T1] raid6: int64x8 gen() 1474 MB/s
[ 3.194434][ T1] raid6: int64x8 xor() 731 MB/s
[ 3.262431][ T1] raid6: int64x4 gen() 1583 MB/s
[ 3.330416][ T1] raid6: int64x4 xor() 789 MB/s
[ 3.398432][ T1] raid6: int64x2 gen() 1357 MB/s
[ 3.466424][ T1] raid6: int64x2 xor() 728 MB/s
[ 3.534429][ T1] raid6: int64x1 gen() 1031 MB/s
[ 3.602421][ T1] raid6: int64x1 xor() 526 MB/s
[ 3.604540][ T1] raid6: using algorithm neonx8 gen() 2260 MB/s
[ 3.610671][ T1] raid6: .... xor() 1671 MB/s, rmw enabled
[ 3.616360][ T1] raid6: using neon recovery algorithm
[ 3.625193][ T1] xor: measuring software checksum speed
[ 3.631813][ T1] 8regs : 2522 MB/sec
[ 3.637415][ T1] 32regs : 2906 MB/sec
[ 3.643676][ T1] arm64_neon : 2434 MB/sec
[ 3.645883][ T1] xor: using function: 32regs (2906 MB/sec)
[ 3.690947][ T1] Btrfs loaded, crc32c=crc32c-generic
[ 3.765196][ T1] imx-xcvr sound-xcvr: snd_soc_register_card failed: -517
[ 3.798398][ T1] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 3.805990][ T1] Bus freq driver module loaded
[ 3.862321][ T1] usbcore: registered new interface driver snd-usb-audio
[ 3.944659][ T1] kvm: exiting hardware virtualization
[ 3.949161][ T1] reboot: Restarting system▒
U-Boot SPL 2021.04-00001-g302084ead7-dirty (May 10 2022 - 02:16:02 +0530)

0 项奖励
回复
2 回复数

1,996 次查看
2744194
Contributor II

Hello @Zhiming_Liu ,

I have same error also. How can I remove kvm function ?

regards.

0 项奖励
回复

2,557 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @swapnilpendhare 

You can try to remove kvm function as the last log shows that kvm failed.

0 项奖励
回复