Hi all,
I am porting android to i.MX51 BBG platform.
I followed i.MX_Android_R10.4_User_Guide and built the android.
But Android Gui is not starting on dvi monitor.
I am sure I am giving correct bootargs.
The log is as below
Later I built the Android by using below command
make PRODUCT-imx51_BBG-eng I am able to get Android GUI but all applications failing. The log file is attached as eng.cap Please can anyone tell me how can I fix it. eng.cap
Original Attachment has been moved to: 166-from_bootup.cap
Sorry for late reply.
Thank you Nitin. I will update after trying.
Just try to take some help from below link also and check your display settings from linux command prompt.
I think Your Laucher is getting failed to load due to some reason thats why you are not getting GUI.
And as per your log you are getting below error so many places.
"E/AndroidRuntime( 2434): FATAL EXCEPTION: launcher-loader"
So i suspect that some library is missing for Launcher.
Try to do all the steps again from begging including flashing of SDCARD.
And try once to make screen time out also more with the help of below link before doing it freshly.
http://osdir.com/ml/android-porting/2011-08/msg00182.html
May be your system is going in suspend mode before lauching the laucher itself.
Do I have to copy userdata.img to SD card?
As GUI starts, after some seconds those error messages pops up.
Thank you.............
Android GUI is starting But below errors are getting displayed.
The process android.process.media has stopped unexpectedly. Please try again.
The process android.process.music has stopped unexpectedly. Please try again.
When I press F1 button It takes me to Menu but when I click on settings it shows the error message of failing application.
You need to do any of the key mapping first for waking up the device from suspend mode.
and if android GUI comes properly you can make screen timeout more and stay awake option you can enable inside settings.
or you can try to increase timeout value also with the help of below link.
Once the Android GUI starts on DVI monitor I see android.process.media failing...
After some minutes system is going to suspend state. How to solve this?
Thanx
Sorry Its the standard board I received from customer.
if it is not a standard EVK of IMX51 from freescale than you may need to change the memory related boot args.
Just try to increase one by one memory related bootargs values like for pmem,fbmem,gpu_memory.
LCD is not connected. Its booting on DVI monitor.
I have tried below bootargs also
console=ttymxc0 init=/init androidboot.console=ttymxc0 di0_primary pmem=32M,64M fbmem=5M gpu_memory=32M video=mxcdi0fb:RGB24,1024x768M@60
console=ttymxc0 init=/init androidboot.console=ttymxc0 di0_primary pmem=32M,64M fbmem=10M gpu_memory=32M video=mxcdi0fb:RGB24,1024x768M@60,bpp=32
sorry i sent wrongly for testing last time.
please try below bootargs once if not tried and tell me.
console=ttymxc0 init=/init androidboot.console=ttymxc0 di0_primary pmem=32M,64M fbmem=10M gpu_memory=32M video=mxcdi0fb:RGB24,1024x768M@60,bpp=32
and tell me which kernel config file(name) you are using for compilation.