Hi I'm using custom board which mcu is imx6sl . Now, emmc can read like p1 p2 p4 but can't mount fs.
Can't anyone tell me the reason? Here is the log:
Starting kernel ...
Initializing cgroup subsys cpuset
Initializing cgroup subsys cpu
Linux version 3.0.35-06522-g0a3529b-dirty (root@HP-Z230-Workstation) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #6 PREEMPT Thu May 12 15:47:06 CST 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6SoloLite EVK Board
Memory policy: ECC disabled, Data cache writeback
CPU identified as i.MX6SoloLite, silicon rev 1.2
On node 0 totalpages: 511999
free_area_init_node: node 0, pgdat c0cb1074, node_mem_map c187a000
Normal zone: 1344 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 170688 pages, LIFO batch:31
HighMem zone: 2752 pages used for memmap
HighMem zone: 337215 pages, LIFO batch:31
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 507903
Kernel command line: console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale androidboot.serialno=0b27b1d4df669563
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1999MB = 1999MB total
Memory: 2016064k/2016064k available, 81084k reserved, 1359868K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xea800000 - 0xf2000000 ( 120 MB)
lowmem : 0xc0000000 - 0xea000000 ( 672 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0038000 ( 192 kB)
.text : 0xc0038000 - 0xc0c4d91c (12375 kB)
.data : 0xc0c4e000 - 0xc0cb1c20 ( 400 kB)
.bss : 0xc0cb1c44 - 0xc0ddee28 (1205 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
*************reg:0xc0011740*********
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
NET: Registered protocol family 16
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :0
->bus_num 0:0 rt9428:0x36
->bus_num 0:1 rt9428:0x36
->bus_num 0:2 tps65185:0x68
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :1
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :2
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :3
->bus_num 0:0 pfuze100:0x8
arch/arm/mach-mx6/board-mx6sl_evk.c:mx6_evk_init
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 262144 B
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
i2c i2c-0: Failed to register i2c client rt9428 at 0x36 (-16)
i2c i2c-0: Can't create device at 0x36
mc_pfuze 0-0008: ID: 0,Full lay: 2 ,Metal lay: 1
mc_pfuze 0-0008: FAB: 0 ,FIN: 0
->pfuze100_init
->pfuze100 version:21
->pfuze100 VGEN1 CTL:18
->pfuze100 VGEN1 VOLT:0
->pfuze100 VGEN1 VOLT:0
->pfuze100 VGEN1 CTL:18
->pfuze100 init end
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
NET: Registered protocol family 23
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
-----------tps65185_probe---------
client->name = tps65185, client->addr = 0x68
tps65185 0-0068: tps65185 write reg:a failed!
i2c-core: driver [tps65185] using legacy suspend method
i2c-core: driver [tps65185] using legacy resume method
rt9428 0-0036: read reg 0x8 io fail
rt9428 0-0036: read device id fail or id is not correct
i2c-core: driver [rt9428] using legacy suspend method
i2c-core: driver [rt9428] using legacy resume method
Switching to clocksource mxc_timer1
FS-Cache: Loaded
CacheFiles: Loaded
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 484K
etb: probe of etb failed with error -2
etm: probe of etm.0 failed with error -2
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = ea820000 suspend_iram_base=ea840000
PM driver module loaded
IMX usb wakeup probe
the wakeup pdata is 0xe60dada0
add wake up source irq 75
IMX usb wakeup probe
the wakeup pdata is 0xe60daba0
cpu regulator mode:ldo_bypass
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
audit: initializing netlink socket (disabled)
type=2000 audit(0.600:1): initialized
highmem bounce pool size: 64 pages
ashmem: initialized
NTFS driver 2.1.30 [Flags: R/O].
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.16)
msgmni has been set to 1282
NET: Registered protocol family 38
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
RTL871X: module init start
RTL871X: rtl8189es v4.3.10_12447.20141008
RTL871X: build time: May 12 2016 15:42:09
RTL871X: module init ret=0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
usb usb1: usb_autoresume_device: cnt 5 -> 1
usb usb1: usb_autoresume_device: cnt 6 -> 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usb usb1: usb_autosuspend_device: cnt 4 -> 0
usb usb1: usb_autosuspend_device: cnt 3 -> 0
add wake up source irq 74
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 74, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
usb usb2: usb_autoresume_device: cnt 5 -> 1
usb usb2: usb_autoresume_device: cnt 6 -> 1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usb usb2: usb_autosuspend_device: cnt 4 -> 0
hub 1-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0
hub 1-0:1.0: usb_autopm_get_interface: cnt 2 -> 1
usb usb2: usb_autosuspend_device: cnt 3 -> 0
hub 1-0:1.0: usb_autopm_put_interface: cnt 0 -> 0
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
imx6 usb charger online:0
android_usb gadget: Mass Storage Function, version: 2009/09/11
hub 2-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0
hub 2-0:1.0: usb_autopm_get_interface: cnt 2 -> 1
hub 2-0:1.0: usb_autopm_put_interface: cnt 0 -> 0
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
USB Host suspend begins
will suspend roothub and its children
hub 1-0:1.0: usb_suspend_interface: status 0
ehci_fsl_bus_suspend begins, DR
ehci_fsl_bus_suspend ends, DR
usb usb1: usb_suspend_device: status 0
usb usb1: usb_suspend_both: status 0
host suspend ends
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
dr_controller_run: udc out low power mode
USB Gadget resume ends
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
-----code:102 val:0-----
-----code:114 val:1-----
-----code:115 val:0-----
-----code:105 val:0-----
-----code:106 val:0-----
add wake up source irq 103
add wake up source irq 104
----------pen probe-------------------
---uart clk is:80000000-----------
-----pen_tablet_init--------
imx-uart.1: ttymxc1 at MMIO 0x2024000 (irq = 59) is a IMX
---------uart2 init---------
--------serial_8250_probe:616---------
-------startup303----usr1:0x2040, usr2:0x4008---------
--------serial_8250_startup:305---------
UCR1:0
UCR2:1
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:4008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:323---------
UCR1:1
UCR2:1
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:4008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:327---------
UCR1:1
UCR2:6027
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:331---------
UCR1:1
UCR2:6027
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:341---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:351---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:356---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:360---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:364---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:1be5
UBRC:4
UTS:60
--------serial_8250_startup:368---------
UCR1:601
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:1be5
UBRC:4
UTS:60
--------serial_8250_startup:372---------
-------startup376----usr1:0x2040, usr2:0x5008---------
setting trigger mode 2 for irq 121 failed (gic_set_type+0x0/0xfc)
Cannot request hw tablet pen IRQ
hw_tablet: probe of hw_tablet.0 failed with error -22
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
Error: Driver 'rt9428' is already registered, aborting...
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
fsl-usb2-udc fsl-usb2-udc: Plug Contact = 1
-----------tps65185_sensor_probe---------
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
fsl-usb2-udc fsl-usb2-udc: It is a stardard downstream port
charger is SDP
imx6 usb charger online:1
sdhci sdhci-esdhc-imx.2: no write-protect pin available!
sdhci sdhci-esdhc-imx.2: no card-detect pin available!
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
Galcore version 4.6.9.9754
Thermal calibration data is 0x5945175f
Thermal sensor with ratio = 185
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
android_work: did not send uevent (0 0 (null))
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
card->ext_csd.rev >= 6 ext_csd.rev = 7
mmc_init_card card->csd.mmca_vsn = 4
mmc_init_card idx = 0
ALSA device list:
No soundcards found.
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
mmc_init_card mmc_switch card speed = 52000000
mmc_init_card mmc_switch idx err = 0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
xt_time: kernel timezone is -0000
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
android_work: sent uevent USB_STATE=CONNECTED
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
android_work: sent uevent USB_STATE=DISCONNECTED
Initializing XFRM netlink socket
NET: Registered protocol family 10
Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
mmc0: new high speed DDR MMC card at address 0001
NET: Registered protocol family 17
NET: Registered protocol family 15
lib80211: common routines for IEEE802.11 drivers
mmcblk0: mmc0:0001 008G70 7.28 GiB
mmcblk0boot0: mmc0:0001 008G70 partition 1 4.00 MiB
mmcblk0boot1: mmc0:0001 008G70 partition 2 4.00 MiB
lib80211_crypt: registered algorithm 'NULL'
lib80211_crypt: registered algorithm 'WEP'
lib80211_crypt: registered algorithm 'CCMP'
lib80211_crypt: registered algorithm 'TKIP'
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
android_work: sent uevent USB_STATE=CONNECTED
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
DVFS driver module loaded
MXCFB_SET_WAVEFORM_MODES:4018462b
MXCFB_SET_TEMPERATURE:4004462c
MXCFB_SET_AUTO_UPDATE_MODE:4004462d
mmcblk0: p4 size 13017088 extends beyond EOD, truncated
MXCFB_SEND_UPDATE:4040462e
MXCFB_WAIT_FOR_UPDATE_COMPLETE:c008462f
MXCFB_SET_PWRDOWN_DELAY:40044630
MXCFB_GET_PWRDOWN_DELAY:80044631
MXCFB_SET_UPDATE_SCHEME:40044632
MXCFB_GET_WORK_BUFFER:c0044634
imx_epdc_fb imx_epdc_fb: ---resolution 1200x825, bpp 16
mmcblk0boot1: unknown partition table
imx_epdc_fb imx_epdc_fb: ---xres: 1216, yres:896, max:1089536
imx_epdc_fb imx_epdc_fb: ---xres: 832, yres:1280, max:1064960
imx_epdc_fb imx_epdc_fb: ---buf_size allocate: 2179072, x_mem_size:0
imx_epdc_fb imx_epdc_fb: ---map_size allocate: 6537216, num_screen:3
mmcblk0boot0: unknown partition table
imx_epdc_fb imx_epdc_fb: ---screen_base allocated at ff400000:0xff400000, 0xa7000000
imx_epdc_fb imx_epdc_fb: ---EPDC version = 21
imx_epdc_fb imx_epdc_fb: ---upd_list[0]:0xe6a072a0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[1]:0xe6a072c0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[2]:0xe6a07800, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[3]:0xe6001980, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[4]:0xe6a07720, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[5]:0xe6a07540, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[6]:0xe6a07760, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[7]:0xe6a07780, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[8]:0xe6a077a0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[9]:0xe6a077c0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[10]:0xe6a07740, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[11]:0xe6a076e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[12]:0xe6001660, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[13]:0xe60016c0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[14]:0xe6a077e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[15]:0xe6a07f20, size: 20
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
imx_epdc_fb imx_epdc_fb: ---upd_list[16]:0xe6a07ee0, size: 20
android_work: sent uevent USB_STATE=CONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[17]:0xe6a07e80, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[18]:0xe6a07e40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[19]:0xe6a07e20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[20]:0xe6a07ec0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[21]:0xe6a07f00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[22]:0xe6a07e00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[23]:0xe6a07e60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[24]:0xe6a07ea0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[25]:0xe6a07de0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[26]:0xe6a07dc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[27]:0xe6a07da0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[28]:0xe6a07d80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[29]:0xe6a07d60, size: 20
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
imx_epdc_fb imx_epdc_fb: ---upd_list[30]:0xe6a07d20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[31]:0xe6a07d00, size: 20
android_work: sent uevent USB_STATE=CONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[32]:0xe6a07cc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[33]:0xe6a07ca0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[34]:0xe6a07c80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[35]:0xe6a07c60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[36]:0xe6a07ce0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[37]:0xe6a07d40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[38]:0xe6a07c40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[39]:0xe6a07c20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[40]:0xe6a07c00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[41]:0xe6a07be0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[42]:0xe6a07bc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[43]:0xe6a07ba0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[44]:0xe6a07b80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[45]:0xe6a07b60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[46]:0xe6a07b40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[47]:0xe6a07b00, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[48]:0xe6a07ac0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[49]:0xe6a07aa0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[50]:0xe6a07a80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[51]:0xe6a07a60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[52]:0xe6a07ae0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[53]:0xe6a07b20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[54]:0xe6a07a40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[55]:0xe6a07a20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[56]:0xe6a07a00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[57]:0xe6a079e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[58]:0xe6a079c0, size: 20
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
imx_epdc_fb imx_epdc_fb: ---upd_list[59]:0xe6a07980, size: 20
android_work: sent uevent USB_STATE=CONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[60]:0xe77ff920, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[61]:0xe77ff8e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[62]:0xe77ff8c0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[63]:0xe77ff8a0, size: 20
imx_epdc_fb imx_epdc_fb: ---size of void*:4, sizeof dma:4, max_num_buffers:2
imx_epdc_fb imx_epdc_fb: ---upd_buf0 virt:0xE6A07960, phys:0xE6A079A0
imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE6C00000, phys:0xA6C00000, PHYS_OFFSET:80000000
imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE6E00000, phys:0xA6E00000, PHYS_OFFSET:80000000
imx_epdc_fb imx_epdc_fb: ---copy 0xFF100000,phys_copy:0xA7800000, working:0xFEF00000, working_phys0xa7c00000,work size:1980000
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
imx_epdc_fb imx_epdc_fb: --num_luts:64 -lut:0xE64771E0, size u32*: 4
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
android_work: sent uevent USB_STATE=CONNECTED
imx_epdc_fb imx_epdc_fb: ---lut_map:0xe64770e0
tps65185 0-0068: Vcom set : -1650 mV
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 2015-01-02 11:22:16 UTC (1420197736)
Freeing init memory: 192K
usb usb1: usb_suspend_both: status 0
hub 2-0:1.0: usb_suspend_interface: status 0
ehci_fsl_bus_suspend begins, Host 1
ehci_fsl_bus_suspend ends, Host 1
usb usb2: usb_suspend_device: status 0
usb usb2: usb_suspend_both: status 0
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init: /dev/hw_random not found
keychord: using input dev gpio-keys for fevent
Hi Ning
seems you used image built for some other than i.MX6SL EVK
board and with different EPD lcd. For i.MX6SL EVK with EPD boot parameters
should be:
setenv bootargs console=ttymxc0,115200 init=/init androidboot.console=ttymxc0
max17135:pass=2,vcom=-2030000 video=mxcepdcfb:E060SCM,bpp=16
please check Android R13.5 documentation on
Supporting Information (16)
i.MX 6 Sololite Android GA BSP Documentation. (REV R13.5)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Devaraja
Actually, the root cause is not found. what i do is just to try to use two different version of tools, and found it can solve the problem. so i think it might be releated with that bin file.
Maybe you can also try this way. "Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER" and "Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER", they can be downloaded from website. if one is not ok, try another one, ..., use them interactively.
Anyway, i'm not sure it is help for you, but you can try
https: //community.freescale.com/thread/324340