[Android] blank sd card format issue on BSP 4.2.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Android] blank sd card format issue on BSP 4.2.2

Jump to solution
3,726 Views
charleshuang
Senior Contributor II

Hi,

We find a sd card format issue on BSP 4.2.2. This issue can be also reproduced on Freescale demo board.

The reproduce steps are as follows.

1. Insert a unformat SD card. For example, use 'fdisk' to delete all the partitions on SD card first, and then just insert into Android system.

2. It will show "blank sd card" notification at left-top corner.

3. Click the notification and it will pop up a dialog to tell you can format this sd card.

4. Click to "Format"

After that, the system will crash.

Here is the logcat for reference.

===

06-05 07:30:30.854 I/ActivityManager( 2509): START u0 {cmp=com.android.systemui/com.android.internal.app.ExternalMediaFormatActivity bnds=[48,76][528,140]} from pid -1

06-05 07:30:30.854 W/ActivityManager( 2509): startActivity called from non-Activity context; forcing Intent.FLAG_ACTIVITY_NEW_TASK for: Intent { flg=0x800000 cmp=com.android.systemui/com.android.internal.app.ExternalMediaFormatActivity bnds=[48,76][528,140] }

06-05 07:30:30.864 W/KeyguardViewMediator( 2509): verifyUnlock called when not externally disabled

06-05 07:30:30.874 D/ExternalMediaFormatActivity( 2634): onCreate!

06-05 07:30:30.964 E/BufferQueue( 2220): [com.android.systemui/com.android.internal.app.ExternalMediaFormatActivity] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

06-05 07:30:31.034 I/ActivityManager( 2509): Displayed com.android.systemui/com.android.internal.app.ExternalMediaFormatActivity: +162ms

06-05 07:30:31.164 D/PhoneStatusBar( 2634): disable: < expand icons* alerts ticker* system_info back home recent clock* search >

06-05 07:30:33.934 W/audio_hw_primary( 2223): do_out_standby... 1075713192

06-05 07:30:34.434 W/audio_hw_primary( 2223): hdmi: card 1, port 0 device 0x400

06-05 07:30:34.434 W/audio_hw_primary( 2223): rate 44100, channel 2 period_size 0x300

06-05 07:30:34.444 W/dalvikvm( 2509): threadid=11: thread exiting with uncaught exception (group=0x417bf930)

06-05 07:30:34.444 W/MountService( 2509): getVolumeState(/storage/emulated/legacy): Unknown volume

06-05 07:30:34.494 D/dalvikvm( 2509): GC_CONCURRENT freed 252K, 54% free 4762K/10328K, paused 3ms+5ms, total 52ms

06-05 07:30:34.494 D/dalvikvm( 2509): WAIT_FOR_CONCURRENT_GC blocked 42ms

06-05 07:30:34.494 D/dalvikvm( 2509): WAIT_FOR_CONCURRENT_GC blocked 43ms

06-05 07:30:34.494 E/AndroidRuntime( 2509): *** FATAL EXCEPTION IN SYSTEM PROCESS: android.server.ServerThread

06-05 07:30:34.494 E/AndroidRuntime( 2509): java.lang.RuntimeException: binder: release 2509:2509 transaction 25160 in, still active

Unable to start service com.androbinder: send failed reply for transaction 25160 to 2860:2860

id.internal.os.storage.ExternalStbinder: release 2509:2749 transaction 25127 in, still active

orageFormatter@41cb5f00 with Intebinder: send failed reply for transaction 25127 to 2634:2634

nt { act=com.android.internal.os.storage.FORMAT_ONLY cmp=android/com.android.internal.os.storage.ExternalStorageFormatter }: java.lang.IllegalArgumentException

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.app.ActivityThread.handleServiceArgs(Actbinder: 2634:2634 transaction failed 29189, size 104-4

ivityThread.java:2673)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.app.ActivityThread.access$1900(ActivityThread.javbinder: 2860:2860 transaction failed 29189, size 276-8

a:141)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1331)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.os.Handler.dispatchMessage(Handler.java:99)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.os.Looper.loop(Looper.java:137)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at com.android.server.ServerThread.run(SystemServer.java:1010)

06-05 07:30:34.494 E/AndroidRuntime( 2509): Caused by: java.lang.IllegalArgumentException

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at com.android.server.MountService.getVolumeState(MountService.java:1499)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at com.android.server.MountService.unmountVolume(MountService.java:1523)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at com.android.internal.os.storage.ExternalStorageFormatter.updateProgressState(ExternalStorageFormatter.java:156)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at com.android.internal.os.storage.ExternalStorageFormatter.onStartCommand(ExternalStorageFormatter.java:97)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     at android.app.ActivityThread.handleServiceArgs(ActivityThread.java:2656)

06-05 07:30:34.494 E/AndroidRuntime( 2509):     ... 5 more

===

Thanks,

Daniel

Labels (2)
0 Kudos
Reply
1 Solution
3,196 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This can be closed

View solution in original post

0 Kudos
Reply
4 Replies
3,197 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This can be closed

0 Kudos
Reply
3,200 Views
danielhung
Contributor III

Hello Freescale,

Does any one can support this issue?

Thanks!

0 Kudos
Reply
3,198 Views
PeterChan
NXP Employee
NXP Employee

Hello Daniel,

The exception is caused by the Android attempts to format an invalid volume. Attached is my patch to solve this issue. Would you please take a try?

Thanks,

Peter

0 Kudos
Reply
3,198 Views
weikeng-jimmy
Contributor III

Hi Sir,

Thanks , it's can fix the issue.

0 Kudos
Reply