Android User's Guide Rev. N7.1.1_1.0.0, 03/2017

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android User's Guide Rev. N7.1.1_1.0.0, 03/2017

Jump to solution
476 Views
hiroyukihara
Contributor III

6.1.6 Booting from SD on the i.MX 7Dual SABRE-SD board

It is written as follows.

Download mode (MFGTool mode)SW4: 00100000 (from 1-8 bit)
Boot_Mode: 01 (from 1-2 bit)
SD bootSW4: 00111000 (from 1-8 bit)
Boot_Mode: 10 (from 1-2 bit)

To boot from SD, perform the following operations:
Chang the board Boot_Mode switch to 10 (from 1-2 bit) and SW4 00100000 (from 1-8 bit).

I think that SW4: 00111000 (from 1-8 bit) is the correct answer.

Which is the correct answer?

AndroidTM Quick Start Guide Rev. N7.1.1_1.0.0, 03/2017

It is written as follows P.31

9. Change SW3 (boot mode) to 10 (from 1 bit to 2 bit). Change SW2 to switch the board back to SD4 boot mode
00100000 (SD), 01010000 (eMMC), 011XXXX0 (NAND).

0 Kudos
1 Solution
371 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The schematic (linked below) shows SW2 should be set as 00100000 to boot SD1

Design files for i.MX 7Dual 

Summary page :

i.MX 7Dual SABRE Board|NXP 

mx7d_boot.jpg

Have a great day,
Yuri
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
372 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The schematic (linked below) shows SW2 should be set as 00100000 to boot SD1

Design files for i.MX 7Dual 

Summary page :

i.MX 7Dual SABRE Board|NXP 

mx7d_boot.jpg

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos