Android Pie - Wifi Integration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Pie - Wifi Integration

1,327 Views
achyut_hegde
Contributor III

Hello,

I can see that, android pie is ported for NXP platforms. I am currently running imx6 with chipset from Marvell.

Which platform is used by NXP for verifying the wifi integration? I would like to use it as a reference point for integrating Marvell. Could you please share the steps/application note for the same if it is present.

Thanks

0 Kudos
Reply
2 Replies

1,217 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Achyut,

The android P is for MX8 and it doesn´t support marvell wifi it support Qualcomm and broadcom devices.

Regards

0 Kudos
Reply

1,217 Views
achyut_hegde
Contributor III

Thanks for the reply.

Could you please share any steps / changes need to migrate a wifi module from Oreo to Pie?

One more clarification needed.

Does the image shared in the website has the changes needed to integrate broadcom and qcom wifi chipsets?

Best regards

Achyut

0 Kudos
Reply