Android Patch Error: M6.0.1_2.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Patch Error: M6.0.1_2.1.0

1,938件の閲覧回数
bhaveshmoradiya
Contributor II

Hi,

I am trying to build Android M6 For my i.Mx6qp Sabre SD board. I followed the instruction avail in Android 6 documents (Android User's Guid Rev. M6.0.1_1.0.0, 04/2016).

Downloaded release package: android_M6.0.1_2.1.0_source.tar.gz

Getting Android Source code: 

http://storage.googleapis.com/git-repo-downloads/repo

https://android.googlesource.com/platform/menifest/+/refs/heads -b android-6.0.1_r3

git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

git checkout m6.0.1_2.1.0-ga 

clone git://git.freescale.com/imx/uboot-imx.git uboot-imx

git checkout m6.0.1_2.1.0-ga

Patch:

source /opt/android_M6.0.1_2.1.0_source/code/M6.0.1_2.1.0/and_patch.sh

c_patch /opt/android_M6.0.1_2.1.0_source/code/M6.0.1_2.1.0/ imx_M6.0.1_2.1.0

After Few checking I got the following Error:

fatal: bad object f7cfc2cca15736862e45ebef54776e0dfdffeb16
Error! Base version commit f7cfc2cca15736862e45ebef54776e0dfdffeb16 doesn't exist in git /home/<user>/myandroid/prebuilts/qemu-kernel. Stop

Please Help Me I already Spend Too much time on this to solve this error Even I tried with Different version of source file with M6.0.1_1.0.0. But Same Result.

How to Fix This ?

Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

1,469件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bhavesh Moradiya,

The patches need to match the commit version exactly for them to be applied correctly.

In the case of the M6.0.1_2.1.0 you can see the required commit on the Android User’s Guide from this Android BSP. In this case it would be:

$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-6.0.1_r22

Please give it a try. I hope this helps!

Regards,

0 件の賞賛
返信