Android Oreo not compatible with iMX6Q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Oreo not compatible with iMX6Q?

2,914 Views
suhaskaundinya
Contributor I

Hello,


I just saw they have released Android Oreo for imx8. But I really wanted that for imx6.

Is there any possibility that I can modified it for imx6? or Is the code compatible only for imx8?

BR,

Suhas

Labels (4)
0 Kudos
Reply
4 Replies

1,816 Views
suhaskaundinya
Contributor I

Hello,

I have successfully built the Android Images of Oreo for imx6.

But when I try to built the u-boot images, I get the following error:

scripts/kconfig/conf  --silentoldconfig Kconfig
  CHK     include/config.h
  UPD     include/config.h
  CFG     u-boot.cfg
  GEN     include/autoconf.mk
  GEN     include/autoconf.mk.dep
  CHK     include/config/uboot.release
  UPD     include/config/uboot.release
  CHK     include/generated/version_autogenerated.h
  UPD     include/generated/version_autogenerated.h
  CHK     include/generated/timestamp_autogenerated.h
  UPD     include/generated/timestamp_autogenerated.h
  CC      lib/asm-offsets.s
lib/asm-offsets.c:1:0: error: unknown value 'armv5' for -march
 /*
 ^
make[1]: *** [lib/asm-offsets.s] Error 1
make: *** [prepare0] Error 2

Could anyone assist me on this?

BR,

Suhas R

0 Kudos
Reply

1,816 Views
antonb
Contributor I

Not clear how does the u-boot compilation started. But such error usually happens if cross compilation is run with host compiler. Make sure you run with proper cross-compiler specified.

make ARCH=arm CROSS_COMPILE=<put your compiler path and prefix here>

And also check out/target/product/<build_target>/ for precompiled u-boot images

0 Kudos
Reply

1,816 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello suhas,

>>Is there any possibility that I can modified it for imx6?

Android Oreo for i.mx8 is also to support i.mx6 serials.

Have a nice day!

TIC weidong sun

0 Kudos
Reply

1,816 Views
hidehikotatebay
Contributor I

Dear Wigros Sun,

I interested in this topic.

I want to boot Android Oreo on i.MX6.

But, I couldn't find Android Oreo BSP for i.MX6.

I see following page.

Android OS for i.MX Applications Processors|NXP 

Please, could you taught me how to download the BSP for i.MX6?

Best regards,

0 Kudos
Reply