Android Oreo, Sabre IMX6Q/QP, PFNs busy

cancel
Showing results for 
Search instead for 
Did you mean: 

Android Oreo, Sabre IMX6Q/QP, PFNs busy

2,030 Views
jdepedro
Contributor IV

I am using the SABRE kit (I have one with i.MX6Q and another with i.MX6QP) and I am using the last Android release (Oreo 8.0.0) released by NXP.

When using the system, for example going to the settings menu, I get a lot of graphical lag, and these errors in the kernel log:

[ 263.819436] alloc_contig_range: [32e00, 335ea) PFNs busy
[ 263.863451] alloc_contig_range: [37200, 379ea) PFNs busy
[ 263.870269] alloc_contig_range: [37200, 37aea) PFNs busy
[ 263.876422] alloc_contig_range: [37400, 37bea) PFNs busy
[ 263.882981] alloc_contig_range: [37400, 37cea) PFNs busy
[ 263.889460] alloc_contig_range: [37600, 37dea) PFNs busy
[ 263.979731] alloc_contig_range: [32e00, 335ea) PFNs busy
[ 263.997406] alloc_contig_range: [37f00, 386ea) PFNs busy
[ 264.008030] alloc_contig_range: [38000, 387ea) PFNs busy
[ 264.016250] alloc_contig_range: [38100, 388ea) PFNs busy
[ 264.035584] alloc_contig_range: [38200, 389ea) PFNs busy
[ 264.274224] alloc_contig_range: [32e00, 335ea) PFNs busy
[ 264.285375] alloc_contig_range: [37f00, 386ea) PFNs busy
[ 264.304507] alloc_contig_range: [38000, 387ea) PFNs busy
[ 264.311177] alloc_contig_range: [38100, 388ea) PFNs busy
[ 264.317586] alloc_contig_range: [38200, 389ea) PFNs busy

Is this a known problem? Are there any fixes available for this?

0 Kudos
2 Replies

601 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

This is an expected behavior. This is due to the lack of memory that the system has, an example could be the i.MX8M-EVK where the memory is higher than the i.MX6 en the android oreo image runs well. Unfortunately, the only solution could be through hardware. I apologize for the inconveniences this could give you.

Best Regards,

Diego.  

0 Kudos

601 Views
Sun1z
Contributor III

I don't think it's due to the lack of memory,  I'm running a very simple example in imx yocto GA release, in such circumstances the total used memory is around 200MB only and my system has 2GB memory but this message still prints. I guess as CMA is a SHARED memory pool, there might be some bugs on memory management.

0 Kudos