Android OTA update is not done in android 9 Automotive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android OTA update is not done in android 9 Automotive

跳至解决方案
6,544 次查看
vinothkumars
Senior Contributor IV

Hi,

I am working on IMX8QM with Android 9 Automotive (android_p9.0.0_2.1.1-auto). I trying Android OTA update.

steps I followed for OTA update,

1, build the ota file (update.zip) by using following commands ,

    source build/envsetup.sh

    lunch mek_8q_car-userdebug

    make target-files-package -j4 

   source build/envsetup.sh

   lunch mek_8q_car-userdebug 

   make otapackage -j4 

2, Copy the update.zip file into cache folder

3, execute the following command,

    echo “--update_package=/cache/update.zip” > /cache/recovery/command

    reboot recovery

But, Android update is not done,

following are the some of observation in Android update.

reboot: Restarting system with command 'recovery'

reboot: Restarting system with command ''

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
6,219 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

OTA update (Manually)

1. extract mek_8q_car-ota-eng.zip file and copy payload.pin file to board folder (sdcard)

           cp payload.bin /sdcard/

2. check payload_properties.txt content and replace header section,

update_engine_client --payload=file:///sdcard/payload.bin --update --              headers="FILE_HASH=GLmv0AhSfgDcnPv4w1BNlJ3TUC6irhh39h9lIdiBZ98=
FILE_SIZE=447604714
METADATA_HASH=ytlU2iEBXgExdM7JGBFgus5EII4tzf5Vs2ArmJj43W8=
METADATA_SIZE=58968"

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,219 次查看
pingyuchen
Contributor II

Hi VinothS,

I can update android by using evk_8mq-ota-eng.zip, this file is created by "make otapackage". Then extract it and copy 

payload.bin properties.txt to /sdcard/. You can use java code to update it. I use UpdateEngine class.

Thanks

0 项奖励
回复
6,219 次查看
vinothkumars
Senior Contributor IV

Thank You Pingyu,

We did an OTA update manually as well as using java application (UpdateEngine class).

But, here is the problem is not able to access the USB stick from the application, So, I copied the OTA file into sd card from the USB mass storage. from this, we got some time delay.

Thank You,

Vinoth SK,

Regards,
Vinothkumar Sekar
0 项奖励
回复
6,218 次查看
pingyuchen
Contributor II

Hi VinothS,

I think that you can use the "File" apk's source code as a reference. You can see it at the android table. In it, we can see the USB stick and copy file from it. Maybe it is a permission problem.

Thanks,

0 项奖励
回复
6,219 次查看
vinothkumars
Senior Contributor IV

Thank you Pingyu chen. I will check.

Vinoth S,

Regards,
Vinothkumar Sekar
0 项奖励
回复
6,220 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

OTA update (Manually)

1. extract mek_8q_car-ota-eng.zip file and copy payload.pin file to board folder (sdcard)

           cp payload.bin /sdcard/

2. check payload_properties.txt content and replace header section,

update_engine_client --payload=file:///sdcard/payload.bin --update --              headers="FILE_HASH=GLmv0AhSfgDcnPv4w1BNlJ3TUC6irhh39h9lIdiBZ98=
FILE_SIZE=447604714
METADATA_HASH=ytlU2iEBXgExdM7JGBFgus5EII4tzf5Vs2ArmJj43W8=
METADATA_SIZE=58968"

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
0 项奖励
回复
6,219 次查看
xuantambk
Contributor II

Hi Vinoth,

I did the same as your suggest but.. after reboot Tartget cannot boot anymore...

log:

Trying to boot from MMC1

Authencation key not yet progammed

keylost package magic error, do nothing here !"

Did i missed something when building OTA package...

It look like some key not sign correctly in TrustOS firmware or eMMC.

0 项奖励
回复
6,219 次查看
vinothkumars
Senior Contributor IV

Hi,

Will you please provide your full steps and also please provide the some more info (Android Version  & Processor).

I followed this document (7.2 Implementing OTA update),

         android_p9.0.0_2.1.1-auto-ga_doc/Android_User's_Guide.pdf

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复