Android OS for IMX93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android OS for IMX93

跳至解决方案
2,539 次查看
Ivan_tch
Contributor I

Hi all,

I am starting to work with the IMX93 Evaluation Kit and we were wondering wherever or not it can work with Android OS, I do see that Android is offered for i.MX8 line of processors - but there is no mention of i.MX9 in documentations or forum (as far as I can tell).

Is Android OS BSP for i.MX93 in the works or are there no plans to have Android running on i.MX9?

Thanks in advance,
Ivan

标记 (2)
0 项奖励
回复
1 解答
2,492 次查看
bernhardfink
NXP Employee
NXP Employee

Starting with Android 10 we had to exclude the i.MX devices which do not have a 3D GPU. Even if the CPU power of an i.MX 93 would be ok for a smaller Android based product, there are some Android requirements which are not met, especially the GPU + Extensions.

In the end it would be technically possible to implement it, but from the marketing point of view it doesn't make any sense to create an NXP proprietary Android version.

Regards,
Bernhard.

在原帖中查看解决方案

3 回复数
2,493 次查看
bernhardfink
NXP Employee
NXP Employee

Starting with Android 10 we had to exclude the i.MX devices which do not have a 3D GPU. Even if the CPU power of an i.MX 93 would be ok for a smaller Android based product, there are some Android requirements which are not met, especially the GPU + Extensions.

In the end it would be technically possible to implement it, but from the marketing point of view it doesn't make any sense to create an NXP proprietary Android version.

Regards,
Bernhard.

2,470 次查看
Ivan_tch
Contributor I

Thank you for the clarification Bernhard - makes more sense now

0 项奖励
回复
2,509 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Official release will not support i.MX93, no such plan.


Best Regards
Zhiming