Android OS for IMX93

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android OS for IMX93

Jump to solution
2,454 Views
Ivan_tch
Contributor I

Hi all,

I am starting to work with the IMX93 Evaluation Kit and we were wondering wherever or not it can work with Android OS, I do see that Android is offered for i.MX8 line of processors - but there is no mention of i.MX9 in documentations or forum (as far as I can tell).

Is Android OS BSP for i.MX93 in the works or are there no plans to have Android running on i.MX9?

Thanks in advance,
Ivan

Tags (2)
0 Kudos
Reply
1 Solution
2,407 Views
bernhardfink
NXP Employee
NXP Employee

Starting with Android 10 we had to exclude the i.MX devices which do not have a 3D GPU. Even if the CPU power of an i.MX 93 would be ok for a smaller Android based product, there are some Android requirements which are not met, especially the GPU + Extensions.

In the end it would be technically possible to implement it, but from the marketing point of view it doesn't make any sense to create an NXP proprietary Android version.

Regards,
Bernhard.

View solution in original post

3 Replies
2,408 Views
bernhardfink
NXP Employee
NXP Employee

Starting with Android 10 we had to exclude the i.MX devices which do not have a 3D GPU. Even if the CPU power of an i.MX 93 would be ok for a smaller Android based product, there are some Android requirements which are not met, especially the GPU + Extensions.

In the end it would be technically possible to implement it, but from the marketing point of view it doesn't make any sense to create an NXP proprietary Android version.

Regards,
Bernhard.

2,385 Views
Ivan_tch
Contributor I

Thank you for the clarification Bernhard - makes more sense now

0 Kudos
Reply
2,424 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Official release will not support i.MX93, no such plan.


Best Regards
Zhiming