Android Nougat on IMX6D 1.3 revision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Nougat on IMX6D 1.3 revision

1,492件の閲覧回数
tkwon
Contributor V

Hello, 

I am using IMX6D 1.2 revision with Android Nougat platform. I am planning to migrate to IMX6D 1.3 revision. On the document, https://www.nxp.com/docs/en/engineering-bulletin/EB803.pdf , it is mentioned that the ROM code changed  ROM_API_TABLE_BASE_ADDR and HAB_API. Does it imply that the Android build running on 1.2 does not work on 1.3 ?

Thanks and Regards,

Taehyuk

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,408件の閲覧回数
tkwon
Contributor V

Hi Igor,

Do you mean that the same image running on 1.2 can run on 1.3 without any change ?

Thanks and Regards,

Taehyuk

0 件の賞賛
返信

1,408件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Taehyuk

 

>Do you mean that the same image running on 1.2 can run on 1.3 without any change ?

yes, however recommended to use latest version Android N7.1.2_2.0.0 BSP Documentation

 

Best regards
igor

0 件の賞賛
返信

1,408件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Taehyuk

Android should also work on rev.1.3 without problems.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信