Android Lollipop booting on SabreSD board fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Lollipop booting on SabreSD board fails

1,692 Views
anjalikkrishna
Contributor III

I am trying to boot Android Lollipop 5.0.2 in Freescale MCIMX6Q-SDP board. I have followed the Android User's guide document downloaded from freescale site for bsp download,build operations.

I was able to compile the source code successfully and the generated images are flashed using dd command. But during booting the system is hanging with "binder: 148:148 transaction failed 29189, size 0-0" error . The log is below.

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

mag3110 2-000e: check mag3110 chip ID

input: FreescaleMagnetometer as /devices/virtual/input/input3

input: eCompass as /devices/virtual/input/input4

mag3110 2-000e: mag3110 is probed

input: FreescaleAccelerometer as /devices/virtual/input/input5

mma8x5x device driver probe successfully

imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

mmc2: new high speed SDHC card at address aaaa

Galcore version 5.0.11.25762

mmcblk2: mmc2:aaaa SS04G 3.69 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk2: p4 size 5567104 extends beyond EOD, truncated

mmc3: BKOPS_EN bit is not set

mmc3: new high speed DDR MMC card at address 0001

mmcblk3: mmc3:0001 SEM08G 7.39 GiB

mmcblk3boot0: mmc3:0001 SEM08G partition 1 2.00 MiB

mmcblk3boot1: mmc3:0001 SEM08G partition 2 2.00 MiB

mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB

mmcblk3: p1 p2

mmcblk3boot1: unknown partition table

mmcblk3boot0: unknown partition table

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

wm8962 0-001a: customer id 0 revision D

fsl-hdmi-dai hdmi_audio.17: failed to probe. Load HDMI-video first.

fsl-hdmi-dai: probe of hdmi_audio.17 failed with error -12

input: WM8962 Beep Generator as /devices/soc0/soc.1/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input6

imx-wm8962 sound.28:  wm8962 <-> 202c000.ssi mapping ok

imx-audio-hdmi sound-hdmi.29: initialize HDMI-audio failed. load HDMI-video first!

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (15956 buckets, 63824 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN1: disabling

SWBST: disabling

SW4: disabling

wm8962-supply: disabling

usb_otg_vbus: disabling

regulator-dummy: disabling

imx mcc test is registered.

UBI error: ubi_init: UBI error: cannot initialize UBI, error -19

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input7

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:05:00 UTC (300)

ALSA device list:

  #0: wm8962-audio

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

type=1403 audit(300.720:2): policy loaded auid=4294967295 ses=4294967295

type=1404 audit(300.730:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

fs_mgr: Could not open block device /dev/block/mmcblk3p5 (No such file or directory).

fs_mgr: Could not set up verified partition, skipping!

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=-1

fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk3p4 for mount /data type ext4 )

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=-1

fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p6 at /cache options: nomblk_io_submit error: No such file or directory

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=-1

fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p7 at /device options: (null) error: No such file or directory

init: fs_mgr_mount_all returned an error

init: fs_mgr_mount_all returned unexpected error 255

SELinux: Could not set context for /cache:  Read-only file system

rfkill: BT RF going to : off

init: cannot find '/system/bin/logd', disabling 'logd'

init: cannot find '/system/bin/lmkd', disabling 'lmkd'

binder: 148:148 transaction failed 29189, size 0-0

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'

init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.product.manufacturer'

init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufacturer'

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'

init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'

android_usb: already disabled

mtp_bind_config

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

binder: 148:148 transaction failed 29189, size 0-0

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: 148:148 transaction failed 29189, size 0-0

I also tried with booting the prebuilt images "android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz". This was  booting even though I am getting some similiar prints shown below

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: barrier=1

fs_mgr: __mount(source=/dev/block/mmcblk2p5,target=/system,type=ext4)=0

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p4): recovery complete

EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p6): recovery complete

EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0

rfkill: BT RF going to : off

binder: 157:157 transaction failed 29189, size 0-0

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'

init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

android_usb: already disabled

mtp_bind_config

root@sabresd_6dq:/ # healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

warning: `main' uses 32-bit capabilities (legacy support in use)

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

period 165695543 ,timeout is 165704133, wake up is :0

period 165695543 ,timeout is 165704133, wake up is :0

request_suspend_state: wakeup (3->0) at 15323264001 (1970-01-01 00:00:11.618185001 UTC)

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

acc_open

acc_release

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

binder: undelivered transaction 3155

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

period 66 ,timeout is 0, wake up is :0

mma enable setting active

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

rfkill: BT RF going to : off

rfkill: BT RF going to : on

mxc_bt_rfkill_reset

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

I have added the "androidboot.selinux=disabled androidboot.dm_verity=disabled" as boot argument to make the prebuilt images to boot. But setting the same boot argument in the built image gives no positive result. Any help would be appreciated....

Labels (3)
2 Replies

461 Views
devarajgs
NXP Employee
NXP Employee

Hi,

The default images that you build works for the eMMC but to boot the image from the SD card, you need to follow the below instructions:

3.4.3 Building Android image for the SD card on the SABRE-SD

Board

The default configuration in the source code package takes internal eMMC as the boot storage. It can be changed to make the

SD card in SD Slot 3 as the boot storage as follows:

remove out/target/product/sabresd_6dq/root directory and boot*.img

remove /out/target/product/sabresd_6dq/recovery directory and recovery*.img

remove /out/target/product/sabresd_6dq/system directory and system*.img

$ make BUILD_TARGET_DEVICE=sd

Follow Section 3.4 to build the images.

For more information please refer to the Android_User_Guide.pdf from the documentation section.

Thanks and Regards,

-Devaraj

461 Views
SergioSolis
NXP Employee
NXP Employee

Android 5.0.2 is still in alpha testing and not released to the public yet.

Please contact the FAE that shared the BSP with you to receive support.

0 Kudos