Android Kitkat 4.4.3 Surface flinger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Kitkat 4.4.3 Surface flinger

1,353 次查看
deepanrajanbara
Contributor IV

Hi

Ours is a custom board based on imx6 we are currently using Android Kitkat 4.4.3.The Kernel consist of Android Linux 3.10.53 and root file system consist of kitkat.But as soon as the systems is booted i get a android logo after which the screen becomes blank. when i give logcat to see the android level log.we have noticed  a log stating

W/SurfaceFlinger( 109): Timed out waiting for hw vsync; faking it

is this the reason the android GUI is not coming up or is there any other change need to be done in file system.

Please let me know and thanks in advance.

Thank you,

Deepanraj.A

0 项奖励
回复
1 回复

877 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

please try

Android 4.4.3 Kitkat Patch (KK4.4.3_2.0.1) and KK4.4.3 source code on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX6_KK443_200_ANDROID_SOURCEBSP&appType...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复