Android KK does not boot when build it under ubuntu 14.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android KK does not boot when build it under ubuntu 14.04

1,563 Views
oussama
Contributor III

I have built android kitkat for some I.MX6 board under ubuntu 14.04, however it refuse to boot from nfs and ubifs and display some init error.

When booting from nfs, it show

[    8.144135] init: skipping insecure file '/default.prop'

[    8.152296] init: skipping insecure file '/init.rc'

The issue is that there is some configuration file with write access for the group and android refuse to use them.

This can be  solved by removing the write permission for the group( chmod g-w -R android_fs).

Why do I have to remove manually the write permission of the group?

Labels (2)
0 Kudos
Reply
0 Replies